DSC56F83783&TWR-56F8400

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSC56F83783&TWR-56F8400

ソリューションへジャンプ
4,253件の閲覧回数
Smaug
Contributor I

Hi,

I can use Processor Expert when USING TWR-56F8400, but I cannot create a project with Processor Expert when using DSC56F83783. Is it because 56F83XXX series is not supported?

 

thanks.

0 件の賞賛
返信
1 解決策
4,239件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Smaug,

Unfortunately, the MC56F83xxx does not support Processor Expert, but we have developed SDK package for MC56F83xxx, pls download the SDK package from the link:

https://mcuxpresso.nxp.com/en/welcome

You can download SDK package and use CodeWarrior for MCU ver11.x to compile and debug.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,240件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Smaug,

Unfortunately, the MC56F83xxx does not support Processor Expert, but we have developed SDK package for MC56F83xxx, pls download the SDK package from the link:

https://mcuxpresso.nxp.com/en/welcome

You can download SDK package and use CodeWarrior for MCU ver11.x to compile and debug.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
4,218件の閲覧回数
Smaug
Contributor I

Hi,

Now I am learning LLC Converter, and the Digital Power Control card used is F83783, but I only have routine code of F82748, F83XXX series seems to have no resources. Can you provide me with the CODE of LLC Converter of F83XXX series,

thanks,

0 件の賞賛
返信
4,199件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the link for LLC design, I do not find the source code for MC56F83783.

https://www.nxp.com/design/designs/llc-resonant-converter-with-sync-rectifier:RDLLC56F82748#Design-R...

The LLC solution belongs to solution team, I do not know the policy for the firmware package publishing, pls contact the distributor for the source code of LLC.

If you still can not get the source code after you bought the LLC board, I will ask internally who have the code and the policy.

 

BR

XiangJun Rong

0 件の賞賛
返信
4,188件の閲覧回数
Smaug
Contributor I

Hi,

      I need the source code of LLC  design using F83783 in the manual. My colleague only had the source code of LLC  design using F82748 in the course he attended before. F83783 can't be configured using configuration tools,such as Process Expert and Quick Start, which caused me a bit of trouble.

      So,I would appreciate it if you could provide the source code of F83783 in the screenshots.

thanks.

0 件の賞賛
返信
4,180件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked the AE team of the policy that the LLC firmware can be shared with customer, I will tell you after I get response.

BR

XiangJun Rong

0 件の賞賛
返信
4,152件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the LLC application code based on MC56F83783, hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信