DSC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
4,919 Views
chaozhuang-b500
NXP Employee
NXP Employee

Hi,

Customer want to confirm the detailed function of NOCOMB bit in register PWMA_FCTRL2n. According to DSC MC56F84789 RM's description,

  • when the bit is cleared, the input to shuntdown PWM is combined with fault signal and filtered signals. So does it mean PWM will be shunt down by fault without any delay?
  • when the bit is set, the input to shunt down PWM is just filtered signals. So does it mean PWM will be shuntdown by fault signal with width larger than filter window? And how dose it influence the fault interrupt?

shunanli-b46639

Tags (2)
0 Kudos
Reply
1 Solution
4,694 Views
shunanli-b46639
NXP Employee
NXP Employee

Hi Chao,

The FCTRL20 and FCTRL21 registers were introduced on tag ghzpwm.03.13.00.00.  Becasue MC56F84789 uses tag ghxpwm.03.08.03.01, so it does not have this function.  It seems the documentation is for a newer version of the PWM than is used on MC56F84789.

Besides, Anguilla Silver uses tag ghzpwm.03.12.05.00 so it does not have the FCTRL20 or FCTRL21 registers either.

i.MXRT use tag ghzpwm.03.27.00.01 so it has these two registers.

View solution in original post

0 Kudos
Reply
7 Replies
4,694 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, all,

The documentation team should be notified so that they can remove the section in next version of RM.

BR

XiangJun Rong

0 Kudos
Reply
4,694 Views
mohammad_kamil
NXP Employee
NXP Employee

Hello xiangjun.rong you spoke to documentation team for this changes?

0 Kudos
Reply
4,695 Views
shunanli-b46639
NXP Employee
NXP Employee

Hi Chao,

The FCTRL20 and FCTRL21 registers were introduced on tag ghzpwm.03.13.00.00.  Becasue MC56F84789 uses tag ghxpwm.03.08.03.01, so it does not have this function.  It seems the documentation is for a newer version of the PWM than is used on MC56F84789.

Besides, Anguilla Silver uses tag ghzpwm.03.12.05.00 so it does not have the FCTRL20 or FCTRL21 registers either.

i.MXRT use tag ghzpwm.03.27.00.01 so it has these two registers.

0 Kudos
Reply
4,694 Views
mohammad_kamil
NXP Employee
NXP Employee

Hello Sherman LI, thanks for clarification. 

0 Kudos
Reply
4,694 Views
chaozhuang-b500
NXP Employee
NXP Employee

Hi Sherman,

Thanks a lot. Get it.

0 Kudos
Reply
4,694 Views
mohammad_kamil
NXP Employee
NXP Employee

Hello Chao Zhuang, can you please share screenshot of RM for "NOCOMB bit in register PWMA_FCTRL2n" where it is in MC56F847XXRM. As i dont see this register  and bits in RM.

0 Kudos
Reply
4,694 Views
chaozhuang-b500
NXP Employee
NXP Employee

hello, please find it in the below screenshot. thanks.pastedImage_1.png

0 Kudos
Reply