DSC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
4,948 次查看
chaozhuang-b500
NXP Employee
NXP Employee

Hi,

Customer want to confirm the detailed function of NOCOMB bit in register PWMA_FCTRL2n. According to DSC MC56F84789 RM's description,

  • when the bit is cleared, the input to shuntdown PWM is combined with fault signal and filtered signals. So does it mean PWM will be shunt down by fault without any delay?
  • when the bit is set, the input to shunt down PWM is just filtered signals. So does it mean PWM will be shuntdown by fault signal with width larger than filter window? And how dose it influence the fault interrupt?

shunanli-b46639

标记 (2)
0 项奖励
回复
1 解答
4,723 次查看
shunanli-b46639
NXP Employee
NXP Employee

Hi Chao,

The FCTRL20 and FCTRL21 registers were introduced on tag ghzpwm.03.13.00.00.  Becasue MC56F84789 uses tag ghxpwm.03.08.03.01, so it does not have this function.  It seems the documentation is for a newer version of the PWM than is used on MC56F84789.

Besides, Anguilla Silver uses tag ghzpwm.03.12.05.00 so it does not have the FCTRL20 or FCTRL21 registers either.

i.MXRT use tag ghzpwm.03.27.00.01 so it has these two registers.

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,723 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, all,

The documentation team should be notified so that they can remove the section in next version of RM.

BR

XiangJun Rong

0 项奖励
回复
4,723 次查看
mohammad_kamil
NXP Employee
NXP Employee

Hello xiangjun.rong you spoke to documentation team for this changes?

0 项奖励
回复
4,724 次查看
shunanli-b46639
NXP Employee
NXP Employee

Hi Chao,

The FCTRL20 and FCTRL21 registers were introduced on tag ghzpwm.03.13.00.00.  Becasue MC56F84789 uses tag ghxpwm.03.08.03.01, so it does not have this function.  It seems the documentation is for a newer version of the PWM than is used on MC56F84789.

Besides, Anguilla Silver uses tag ghzpwm.03.12.05.00 so it does not have the FCTRL20 or FCTRL21 registers either.

i.MXRT use tag ghzpwm.03.27.00.01 so it has these two registers.

0 项奖励
回复
4,723 次查看
mohammad_kamil
NXP Employee
NXP Employee

Hello Sherman LI, thanks for clarification. 

0 项奖励
回复
4,723 次查看
chaozhuang-b500
NXP Employee
NXP Employee

Hi Sherman,

Thanks a lot. Get it.

0 项奖励
回复
4,723 次查看
mohammad_kamil
NXP Employee
NXP Employee

Hello Chao Zhuang, can you please share screenshot of RM for "NOCOMB bit in register PWMA_FCTRL2n" where it is in MC56F847XXRM. As i dont see this register  and bits in RM.

0 项奖励
回复
4,723 次查看
chaozhuang-b500
NXP Employee
NXP Employee

hello, please find it in the below screenshot. thanks.pastedImage_1.png

0 项奖励
回复