Code warrior 8.3 compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrior 8.3 compile error

2,018 Views
aksnrks
Contributor I

DSP MC56F8014 projected created from 2 or 3 year back. Now i am open this project in code worrior 8.3 and its ask to migrate the i allow for migrate then project loded and some target error ootput source file not found in project.

Once i compile its given target not found in project.

 

Pls help me guys.

0 Kudos
Reply
2 Replies

1,928 Views
jacob652
Contributor I

Most commonly, you will experience program lock-ups, slow PC performance, system freezes, blue screen errors, startup or shutdown problems, and installation errors. In the worst case, if the DLL is required by Windows, your entire system could become unstable.  

0 Kudos
Reply

2,005 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls new a project based on MC56F8014 with CodeWarrior for DSP56800E ver8.3, then complie/link and download it to flash of MC56F8014.

After above procedures are okay, Then drag the files in the old project to the new project, if you use PE, enable and configure the bean, then compile/link.

I suppose that the CodeWarrior version difference leads to your error, you can not open the old project in the latest version of CW tools.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply