Can only Transmit over the Serial Communication Interface, when connected to Debugger.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can only Transmit over the Serial Communication Interface, when connected to Debugger.

跳至解决方案
4,414 次查看
malikos
Contributor I

I am currently using a MC9S12ZVM Family. I am trying to transmit some data over the serial communication interface (via Lin). However I can only successfully transmit the data when I am connected to Code Warrior and when the debugging session is active. I do not want to use the debugger when transmitting the data (would do it via Canoe). Is there a way of configuring the SCI so that you do not need to use the debugger to send the information over the SCI. 

 

I attach my configuration

标记 (1)
0 项奖励
回复
1 解答
4,352 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

it smells like there is something initialized twice and is allowed to be only once.

You use Processor Expert setup and believe you made some adjustment.

Some registers are write once only. For example MODRR, CPMUCOP register which routes peripherals to pins. When you use normal mode (no BDM) the if it is set for the first time then it is not re-writable.

Moreover, you only describe it does not communicate. Have you tested the MCU is working and not still in the reset phase or in loop start-reset caused by COP setup...write once only?

 

Best regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,353 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

it smells like there is something initialized twice and is allowed to be only once.

You use Processor Expert setup and believe you made some adjustment.

Some registers are write once only. For example MODRR, CPMUCOP register which routes peripherals to pins. When you use normal mode (no BDM) the if it is set for the first time then it is not re-writable.

Moreover, you only describe it does not communicate. Have you tested the MCU is working and not still in the reset phase or in loop start-reset caused by COP setup...write once only?

 

Best regards,

Ladislav

0 项奖励
回复
4,345 次查看
malikos
Contributor I

Great. That was the issue. Writting twice to the MODRR0 rgister

0 项奖励
回复
4,393 次查看
malikos
Contributor I

Any ideas? The serial communication interface is Serial Communication Interface (S12SCIV6)

0 项奖励
回复