CWH-UTP-ONCE-HE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CWH-UTP-ONCE-HE

2,834 次查看
Abdulkerim
Contributor I

I need support device list of CWH-UTP-ONCE-HE programmer
or can you sent me the software by Email
I need to writing and reading these CPU
56F8006, 56F8023, 56F8034 etc...

I will buy this programmer or any other programmer that will help me in my work
Is shipping to Turkey available?

Email: [email protected]

thank you so mutch

标记 (1)
0 项奖励
回复
3 回复数

2,817 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As it's designation 56800E Flash Programmer implies that the tools just writes code/data to flash instead of reading it to a flash, furthermore, reading flash to a file may infringe the code IP, so it is not a main function. I think the CodeWarrior for MCU tools provides the function.

Click the "Add Action", there is "Dump Flash" option, you can download memory to file with the option.

Hope it can help you

BR

Xiangjun Rong

 

xiangjun_rong_0-1619491653102.png

 

0 项奖励
回复

2,820 次查看
Abdulkerim
Contributor I

No problem for a computer system
Because my computer is running on Windows 7 64 bits mainly
But I didn't see that the software had a "reading" icon.
I need to write and read memory for that controller

MC56F8006, 13, 23, 34 and MC56F82746V
Can you advise me
thank you
0 项奖励
回复

2,823 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Abdulkerim,

Pls go to the link:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

and download the