'CCSProtocolPlugin' error when connecting debugger with USB TAP and Codewarrior 11.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'CCSProtocolPlugin' error when connecting debugger with USB TAP and Codewarrior 11.1

2,619 Views
SGatDGI
Contributor I

Hi,

I am using Codewarrior ver11.1 for development of MC56F8367 DSC along with USB TAP for debugging.

I have Windows 11 installed on my computer.

When I try to run the debugger, I am getting the 'CCSProtocolPlugin' error during the connection stage itself.

I am not able to open CCS.exe either to send commands and verify the connection.

Can you please help me resolve this error and understand why the connection would not happen ?

Is Codewarrior 11.1 compatible with windows 11 ?

 

Thank You !

0 Kudos
Reply
3 Replies

2,520 Views
SGatDGI
Contributor I

Hello, 

Yes I am able to see the CCS console opened up now ( by doing ' show Console ' to the minimized CCS Server logo ).

The debugging also works now. Although it requires to power cycle the target in order to get no errors while the debugger is connecting / downloading the code.

 

Thanks !

0 Kudos
Reply

2,605 Views
SGatDGI
Contributor I

If I enable the CCS executable as part of project ( Run/Debug ) properties I see the following in the codewarrior console. The CCSPRotocolPlugin error still remains.

SGatDGI_1-1696010728377.pngSGatDGI_1-1696010728377.png

 

0 Kudos
Reply

2,528 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Have you solved your problem now?

I am sure that the CodeWarrior for MCU ver11.x can work on the Win10 OS.

I have tried to download code to MC56F8367-EVK board, it is okay.

BR

XiangJun Rong

xiangjun_rong_0-1696915468833.pngxiangjun_rong_0-1696915468833.png

 

0 Kudos
Reply