CCCSClient::ResetToDebug: Network timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCCSClient::ResetToDebug: Network timeout

3,106件の閲覧回数
lpineau
Contributor I

We are using USB TAP (900-75116; REV A; 01001362) to debug (via CodeWarrior) and to program (via 56800E Flash programmer) our target DSP 56F8355. CodeWarrior IDE version is 5.9.0 (build 4713) on Windows XP.

Unfortunately, I no longer can program or debug our target:

  • The "TX/RX" led on the USB TAP blinks and the "RUN/PAUSE" led remains RED,
  • An error "CCCSClient::ResetToDebug: Network timeout" is always displayed by Flash Programmer (please find enclosed its log file).

Could you please help to fix this issue.

Thanks in advance for your help.

0 件の賞賛
返信
2 返答(返信)

2,522件の閲覧回数
ingostar
Contributor I

I guess you didn't get any help with this problem. I'm having the same problem with a device that has run smoothly for the last 10 years.

0 件の賞賛
返信

2,923件の閲覧回数
caesar_song
Contributor III

Could you please help to fix this issue. I have meet the issue,

Thanks in advance for your help.

0 件の賞賛
返信