CAN Bootloader 56F8367

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Bootloader 56F8367

1,790件の閲覧回数
ainara
Contributor I

Hello,

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8357, and now I need to load my application via CANBUS.

 

1- What steps is it necessary to realize the load?

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8367 and now I need to load my application:

1 - what steps I have to do to load my application via CANBUS?

2 - How can I modify the BOOT START DELAY via CANBUS?

3 - which CAN -identifiers should be used?

 

I use IXXAT USB-to-CAN compact.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,630件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

Modification of BOOT START DELAY is only at compile time given the design of the boot code.

Do you have the source? If so you can customize it.

0 件の賞賛
返信