CAN Bootloader 56F8367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Bootloader 56F8367

1,786 Views
ainara
Contributor I

Hello,

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8357, and now I need to load my application via CANBUS.

 

1- What steps is it necessary to realize the load?

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8367 and now I need to load my application:

1 - what steps I have to do to load my application via CANBUS?

2 - How can I modify the BOOT START DELAY via CANBUS?

3 - which CAN -identifiers should be used?

 

I use IXXAT USB-to-CAN compact.

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,626 Views
johnlwinters
NXP Employee
NXP Employee

Modification of BOOT START DELAY is only at compile time given the design of the boot code.

Do you have the source? If so you can customize it.

0 Kudos
Reply