CAN Bootloader 56F8367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN Bootloader 56F8367

1,652 次查看
ainara
Contributor I

Hello,

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8357, and now I need to load my application via CANBUS.

 

1- What steps is it necessary to realize the load?

 

Via JTAG I have loaded the CAN bootloader in the DSP56F8367 and now I need to load my application:

1 - what steps I have to do to load my application via CANBUS?

2 - How can I modify the BOOT START DELAY via CANBUS?

3 - which CAN -identifiers should be used?

 

I use IXXAT USB-to-CAN compact.

 

Thanks.

标签 (1)
0 项奖励
回复
1 回复

1,492 次查看
johnlwinters
NXP Employee
NXP Employee

Modification of BOOT START DELAY is only at compile time given the design of the boot code.

Do you have the source? If so you can customize it.

0 项奖励
回复