BLDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC

2,411 Views
1471371112
Contributor I

I can't program, but I need an engineering source to control the BLDC

4 Replies

2,249 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, 建明

I attach the BLDC motor control code based on Hall sensor and TWR-56F8400, TWR-MC-LV3PH, TWR-ELEV, the tools is CodeWarrior for mcu ver10.x,  hope it can help you.

This is DSC family link:

Digital Signal Controllers|NXP 

56F84xxx link:

MC56F84xxx|Digital Signal Controllers|NXP 

BR

Xiangjun rong

0 Kudos
Reply

2,249 Views
Ben
Senior Contributor I

Hello Xiangjun rong,

Do you have a saple code for the 8257 too? 

BR

Benny

0 Kudos
Reply

2,249 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Benny,

I attach the BLDC example code based on MC56F8257, hope it can help you

BR

Xiangjun Rong

2,249 Views
Ben
Senior Contributor I

Hi

Thank you for the fast answer.

Maybe you can help me with my license question too (https://community.nxp.com/thread/485571 ) as nobody responded...

BR

Benny

0 Kudos
Reply