About digital LLC reference design by MC56F8xxxx.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About digital LLC reference design by MC56F8xxxx.

3,369 Views
Redchi
Contributor I

Is there a reference design about digital peak current mode control or bang bang charge control for LLC resonant converter by MCF56F83xxx or MC56F81xxx to implement those?
Digital LLC converter of peak current mode control concept is similar to FAN7688 or NCP1399 analog controller IC.
Digital LLC converter of bang bang charge control concept is similar to TEA2016 controller IC.

Could anyone provide me related docs and source code?

0 Kudos
Reply
7 Replies

3,352 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Red,

I do not know if you use LLC resonant converter layout or general Buck layout with peak current mode control.

If you use LLC resonant converter, pls refer to the link:

https://www.nxp.com/design/designs/llc-resonant-converter-with-sync-rectifier:RDLLC56F82748

The LLC varies  PWM frequency to adjust the output voltage, it does not use peak current control mode. I suppose that peak current control mode is used in current loop with fixed PWM frequency.

BR

XiangJun Rong

 

0 Kudos
Reply

3,343 Views
Redchi
Contributor I

I once received a similar solution on this webinar.

https://www.nxp.com.cn/design/training/%E6%81%A9%E6%99%BA%E6%B5%A6-dsc-%E6%9E%B6%E6%9E%84%E5%8F%8A%E...

Time stamp at 54:40.

Could the nxp provide related documents and source code?

Thanks.

0 Kudos
Reply

3,348 Views
Redchi
Contributor I

Hi xiangiun rong

Thanks your reply.

I think that the LLC converter also can implement peak current mode control(Charge current mode control).

Our layout get the resonant current and integrate it and it will into internal comparator.

When occurs peak current event, It is going to turn off PWM and then we also want to get toff time as some as ton time but we don't know how to implement it.

You can refer as follow. We want to implement below docs method by full digital control via DSC.

https://www.onsemi.com/pdf/datasheet/ncp1399-d.pdf

https://www.mouser.com/datasheet/2/149/FAN7688-760738.pdf

@xiangjun_rong 

 

BR,

Red.

0 Kudos
Reply

3,335 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Red,

From your Email, it appears you are student in a university. The source code is confidential, the product manager is responsible for the distributing the source code and schematics based on business.

You said that you was invited to attend a DSC training by AE, can you contact him to get the source code and schematics?

BR

XiangJun Rong

0 Kudos
Reply

3,333 Views
Redchi
Contributor I

I have been working for 3 years and this NXP account was registered when I was a student, so it is the university mailbox. 

How can I get this source code and docs?

@xiangjun_rong 

0 Kudos
Reply

3,307 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Red,

It is dependent on the business whether the product manager would like to share the solution with you or not. If you want to request the solution, you have to submit your company name, address, country, tel number,project, part number, estimated pcs so that the product manager and FAE can evaluate.

In order to protect customer privacy, you can submit a ticket to the support link.

https://support.nxp.com/s/

 

BR

XiangJun Rong

0 Kudos
Reply

3,300 Views
Redchi
Contributor I

Thanks! @xiangjun_rong 

0 Kudos
Reply