ADC for MC56F83783

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC for MC56F83783

2,153件の閲覧回数
Mariya
Contributor I

I am using MC56F83783 controller.As the controller does not support processor expert.I want an idea  for Single ended sequential ADC with  LOOPING scan mode..

0 件の賞賛
返信
3 返答(返信)

2,119件の閲覧回数
Mariya
Contributor I

Can you provide an application note for mc56f83783 controller, will be helpful going forward.

0 件の賞賛
返信

2,112件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

 

For the application note of MC56F83xxx, pls download from the website:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

Hope it is helpful

BR

XiangJun Rong

0 件の賞賛
返信

2,123件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The PE(Processor Expert) is no longer supported for the MC56F83xxx family, you have to use SDK package which is run on CodeWarrior for MCU ver11.x.

Pls download SDK package from the link:

https://mcuxpresso.nxp.com/en/welcome

 

In the SDK example, there is ADC example, pls try to test it, if you require the looping ADC mode, I suppose you have to modify the ADC example code.

Hope it is helpful

BR

XiangJun Rong

0 件の賞賛
返信