56F84786-AD initial time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56F84786-AD initial time

2,000件の閲覧回数
david_lin
Contributor II

Hi,

I’m debugging the SW on chip 56F84786 .My AD is initialized by PWM val0 output-trigger0. I want to change my AD sample initial time,but I cannot change the PWM val0 value because val0 value has been used by other trigger function. And I also cannot use PWM val1,PWM val2,PWM val3,PWM val4,PWM val5.Can you give some advice?

0 件の賞賛
返信
2 返答(返信)

1,987件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Lin,

I do not know if your ADC triggering signal is required to synchronize with PWM signal from your application requirement.

If it is not required, I suppose that you use ADC12 module, in the case, the ADCA trigger signal is XBAR_OUT12, you can select any signal from the Table 3-6. XBARA and XBARB Inputs in MC56F847xxRM.pdf

xiangjun_rong_0-1621825112299.png

 

If the ADC trigger signal is required to synchronize with PWM signal, and all the PWM VALx are used, in the case it is complex. I do not know if the PWMB module is used, if it is not used, you can synchronize the PWMA and PWMB, use PWMB val0 register to trigger ADC, in the case, the PWMA PWM signals will synchronize with ADC triggering signal.

Hope it can help you

BR

XiangJun Rong

 

 

0 件の賞賛
返信

1,999件の閲覧回数
david_lin
Contributor II

2021-05-22 192048.png2021-05-22 192518.png

タグ(1)
0 件の賞賛
返信