DNPU Training Hub

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DNPU Training Hub

DNPU Training Hub


Restricted Beta Program

The DNPU Training Hub helps you build knowledge and accelerate development with DNPU solutions:

  • Access curated training materials and technical resources
  • Explore use cases, applications, and implementation approaches
  • Utilize presentations, labs, and supporting content to enhance your learning

讨论

排序依据:
Multi-Stream YOLOv8 Object Detection    This post shows a walkthrough of the ARA2 Vision Examples package and its multi-stream YOLOv8 object detection application. The ara2-vision-examples package provides vision AI examples for NXP i.MX platforms using Ara240 DNPU acceleration. It demonstrates real-time video processing with AI/ML inference capabilities such as object detection, classification, pose estimation, and semantic segmentation. This walkthrough focuses on the multistream_yolov8 application, which uses GStreamer to process up to eight simultaneous video streams, run YOLOv8 object detection on each stream, and display the results in a single mosaic view.   Key Features Multi-stream video processing from 1 to 8 streams YOLOv8 object detection accelerated by Ara240 DNPU Support for YOLOv8n, YOLOv8s, YOLOv8m, YOLOv8l, and YOLOv8x models GStreamer-based video pipeline Mosaic display output with bounding boxes Runtime options for stream count, model selection, synchronization, and endpoint selection FPS and IPS performance overlay per stream   Running the Demo   Run the application with the default settings: multistream_yolov8 Run with a specific number of streams: multistream_yolov8 -s 4 Select a different YOLOv8 model: multistream_yolov8 -s 4 --model yolov8s Run eight streams for maximum throughput: multistream_yolov8 -s 8 --sync false Enable synchronized playback: multistream_yolov8 -s 4 --sync true   Walkthrough Video   In the attached video, it is shown how to launch the application, configure the number of streams, select different YOLOv8 models, and view the object detection results in the mosaic display.   Links ARA2 Vision Examples repository: https://github.com/nxp-imx-support/ara2-vision-examples Multi-stream YOLOv8 README: https://github.com/nxp-imx-support/ara2-vision-examples/blob/main/tasks/object-detection/yolov8n/multistream-gstreamer/README.md
查看全文
The Runtime SDK for AI/ML acceleration using the Ara240 NPU on NXP i.MX SoCs, provides the runtime environment for the Ara‑2 NPU.   Main Purpose of the Package    1. Provide the runtime environment for the Ara‑2 NPU This runtime sdk package installs everything needed for an i.MX system to communicate with and utilize the Ara240 NPU hardware, including: NPU drivers  Low‑level utilities (metrics, hardware bring‑up, flash tools) Proxy services that interface applications with the NPU Firmware loaders and NPU configuration files 2. Allow users to run AI/ML inference models on the NPU The Ara240 runtime environment includes tools for: Downloading pre‑compiled AI/ML models Running performance tests on the NPU Running classification, detection, pose, and segmentation models Inspecting HW IPS (inference/second) and real hardware performance   Scripts such as: fetch_models.sh ara_metrics.sh chip_info.sh program_flash.sh run_models_perf.sh 3. Automatically configure and optimize the i.MX system Installation does the following automatically: Expands system partition to handle large models (LLMs/VLMs) Sets up an 8GB SWAP for devices with limited RAM Prepares the runtime environment for AI workloads 4. Manage and update Ara‑2 firmware The package contains scripts to: Check the installed firmware version ( chip_info.sh ) Update firmware if needed ( program_flash.sh ) 5. Provide systemd service for automatic startup The SDK installs: A systemd service: rt‑sdk‑ara2.service   Walkthrough Video Below is the walkthrough video for this package  
查看全文
eIQ AAF Connector   In this post, I want to share a quick walkthrough of eIQ AAF Connector, a REST-based server that enables LLM and VLM inference on NXP i.MX platforms using the Ara240 DNPU. The connector provides a simple HTTP interface for client applications to send prompts and receive streaming token responses from models running locally on Ara240. It is also the communication layer used by applications such as LLM Edge Studio and VLM Edge Studio.   Key Features REST API server for Ara240-accelerated model inference Chat Completions-style HTTP endpoint Streaming token responses Support for text LLMs and Qwen2.5-VL models Model configuration through server_config.json Optional tool calling and guided generation support for compatible text models Optional semantic prompt caching for text models OpenAPI documentation available through the /docs endpoint   How It Works   The eIQ AAF Connector runs on the i.MX host and exposes a REST API. Client applications send prompts to the connector, which communicates with the Ara240 Runtime SDK and the loaded model.dvm running on the Ara240 DNPU. The response is returned as generated tokens, with support for streaming output.   Basic Setup   After installing the Debian package, activate the connector virtual environment: source /usr/share/eiq/aaf-connector/venv/bin/activate Run the connector: connector By default, the server starts on: 127.0.0.1:8000 To allow access from another device, start it with: connector --host 0.0.0.0   Configuration   The connector uses a JSON configuration file named server_config.json to define server settings and available models. This includes model paths, tokenizer paths, model type, prompt size, tool calling support, and whether the model should be loaded at startup. { "log_level": "INFO", "model_config_path": "/usr/share/llm/{}/", "model_tokenizer_path": "/usr/share/llm/{}/tokenizer", "available_models": [ { "name": "qwen2_5-7b", "description": "Qwen2.5 7B instance", "type": "text", "tool_calling": "native", "max_prompt_size": 2047, "enabled": true } ] }   Sending a Test Request   Once the server is running, a basic request can be sent to the chat completions endpoint: curl -H 'Content-Type: application/json' \ -d '{ "model": "Qwen2.5-7B-Instruct", "messages": [ { "role": "user", "content": "Who are you?" } ] }' \ -X POST 0.0.0.0:8000/v1/chat/completions The API can also be tested from the OpenAPI UI at: http://0.0.0.0:8000/docs   Walkthrough Video   In the attached video, I show how to start the eIQ AAF Connector, verify the server is running, configure a model, and send a sample request to the /v1/chat/completions endpoint.   Summary   The eIQ AAF Connector provides the REST API layer for running edge AI models on NXP i.MX platforms with Ara240 DNPU acceleration. It allows applications to send prompts, receive generated responses, and integrate local LLM or VLM inference into demos, prototypes, and edge AI workflows.   Link eIQ AAF Connector repository    
查看全文
VLM Edge Studio   In this post, I want to share a quick walkthrough of VLM Edge Studio, an NXP launcher application designed to interact with supported Vision-Language Models running locally on FRDM i.MX platforms with Ara240 DNPU acceleration. VLM Edge Studio provides a Qt/QML-based GUI for model selection, prompt input, and visual interaction with locally running VLMs at the edge. It communicates with the Ara240 Runtime SDK through the eIQ AAF Connector using a REST-based interface and streaming token responses.   Key Features Local Vision-Language Model inference on supported i.MX platforms Ara240 DNPU acceleration GUI-based model selection and prompt input Streaming token output Integration with eIQ AAF Connector and Ara240 Runtime SDK Support for camera-based visual input using a USB-C HD camera   Supported Model Qwen2.5-VL-7B-Instruct-Ara240 This model is provided as an Ara240-compatible model.dvm file and is intended for local execution on the target platform.   Basic Installation   After making sure the Ara240 Runtime SDK is installed on the target board, copy the Debian package: scp vlm-edge-studio.deb root@<ip_addr>: Install it with: dpkg -i vlm-edge-studio.deb The installation may take a few minutes because the model needs to be extracted during setup.   Running VLM Edge Studio   Start the application with: run_vlm_edge_studio Before launching, make sure the Ara240 runtime service is running: systemctl status rt-sdk-ara2.service --no-pager -l Once the GUI appears, click LOAD to load the model. After the model is ready, enter a prompt and submit it to interact with the VLM locally on the i.MX platform.   Walkthrough Video   In the attached video, I show how to launch VLM Edge Studio, load the supported Vision-Language Model, submit a prompt, and interact with the model running locally with Ara240 DNPU acceleration. Summary   VLM Edge Studio is a useful tool for evaluating local Vision-Language Model inference on NXP i.MX platforms using Ara240 DNPU acceleration. It provides a simple workflow for loading the model, entering prompts, and interacting with visual-language AI directly at the edge.   Link VLM Edge Studio repository  
查看全文
LLM Edge Studio   In this post, I want to share a quick walkthrough of LLM Edge Studio, an NXP launcher application designed to test supported Large Language Models running locally on i.MX platforms with Ara240 DNPU acceleration. LLM Edge Studio provides a simple GUI to select a model, load it, enter prompts, and interact with an LLM directly at the edge. It communicates with the Ara240 Runtime SDK through the eIQ AAF Connector, using a REST-based interface for prompt submission and streaming token responses.   Key Features Local LLM inference on supported i.MX platforms Ara240 DNPU acceleration GUI-based model selection and prompt input Streaming token output Integration with eIQ AAF Connector and Ara240 Runtime SDK Support for prebuilt Debian package installation or building from source   Supported Models Qwen2.5-coder-1.5B Qwen2.5-7B-Instruct These models are provided as Ara240-compatible model.dvm files and are intended for local execution on the target platform.   Basic Installation   After making sure the Ara240 Runtime SDK is installed on the target board, copy the Debian package: scp llm-edge-studio.deb root@<ip_addr>: Install it with: dpkg -i llm-edge-studio.deb The installation may take a few minutes because the required models are downloaded during setup.   Running LLM Edge Studio   Start the application with: run_llm_edge_studio Before launching, make sure the Ara240 runtime service is running: systemctl status rt-sdk-ara2.service --no-pager -l Once the GUI appears, click LOAD to load the selected model. After the model is ready, enter a prompt and submit it to start interacting with the LLM.   Walkthrough Video In the attached video, I show how to launch LLM Edge Studio, load a supported model, submit a prompt, and view the generated response running locally on the i.MX platform with Ara240 DNPU acceleration.   Summary   LLM Edge Studio is a useful tool for quickly evaluating local LLM inference on NXP i.MX platforms using Ara240 DNPU acceleration. It provides a simple workflow for model loading, prompt testing, and observing token streaming directly at the edge. Link LLM Edge Studio repository: https://github.com/nxp-imx-support/llm-edge-studio
查看全文
Smart Device Gateway   In this post, I want to share a quick walkthrough of Smart Device Gateway, a FastAPI-based demo server that allows connected devices to use local GenAI capabilities accelerated by the Ara240 DNPU. The idea behind this demo is to centralize AI intelligence in one gateway instead of adding powerful AI hardware to every device. A connected device only needs a microphone, speaker, and network connection to become a voice-enabled assistant.   What It Does   Smart Device Gateway enables devices such as appliances or embedded clients to send audio to a local server, process the request using speech recognition, RAG, an LLM running on Ara240 DNPU, and text-to-speech, then stream the spoken response back to the client. The current demo showcases intelligent device assistants for a generic oven and coffee machine/barista use case, using device manuals as the knowledge base for contextual responses.   Architecture Overview   The Smart Device Gateway receives audio from a client over WebSocket, converts speech to text, retrieves relevant context from a device knowledge base, sends the prompt to the LLM through the eIQ AAF Connector, converts the generated response back to speech, and streams the audio response to the client. At a high level, the flow is: Audio Input → STT → RAG → eIQ AAF Connector / LLM → TTS → Audio Output The LLM runs on the Ara240 DNPU, while the server runs on the FRDM i.MX platform.   Basic Server Installation   Install the Debian package on the board: dpkg -i smart-device-gateway_1.0.0_all.deb Start the server: run_server_only --host 0.0.0.0 --port 8080 The server expects the eIQ AAF Connector to already be running on 0.0.0.0:8000 with Qwen2.5-7B-Instruct properly configured. Alternatively, the demo can start the server together with the connector: run_server --host 0.0.0.0 --port 8080   Host PC Client Example   The demo includes a push_to_talk client that can run on a host PC. After copying the push_to_talk folder, run: python -m uv run push_to_talk.py --server_ip <BOARD_IP> --port <PORT> --device oven You can also use: python -m uv run push_to_talk.py --server_ip <BOARD_IP> --port <PORT> --device barista If no device name is provided, the RAG knowledge base is not used and the response is generated from the LLM’s general knowledge.   Walkthrough Video   In the attached video, I show how to start the Smart Device Gateway server, connect a client, select a device profile such as oven or barista, ask a voice question, and receive a spoken response generated locally using Ara240 DNPU acceleration.     Summary   Smart Device Gateway demonstrates how everyday devices can become voice-enabled assistants by connecting to a local AI gateway. By combining STT, RAG, LLM inference on Ara240 DNPU, and TTS, the demo provides a practical reference for building local, privacy-focused GenAI experiences on NXP i.MX platforms.   Link Smart Device Gateway repository    
查看全文
Applies to: LLM Edge Studio Go Point Demo Workaround: Requires custom llm_params configuration The model Qwen2.5-Coder-1.5B is not supported out-of-the-box in LLM Edge Studio using the default configuration. The model loading will fail when attempting to run the model with the default  server_config.json fix: update the  llm_params  section in  server_config.json  with compatible sampling values: - Open config file: vi llm-edge-studio/usr/share/llm-edge-studio/server_config.json - Replace the parameters as follows: "llm_params": { - "temperature": 0.0, - "top_k": 0, - "top_p": 0.0, + "temperature": 1.0, + "top_k": 50, + "top_p": 0.95 } Qwen2.5-Coder-1.5B should run with proper output quality and sampling behavior after applying the updated configuration.  Remarks:  This configuration enables proper behavior for Qwen2.5-Coder-1.5B It may generate warning messages when running Qwen2.5-Instruct-7B, but the model will continue to function normally BR,
查看全文
  Applies to: VLM Edge Studio Demo using Qwen‑VL backend Workaround: Apply the attached  apply_qwenvl_fix.sh  script   In the current VLM Edge Studio Demo, users may encounter a runtime failure when starting the Qwen‑VL Vision Language Model. The issue is caused by incorrect processor initialization, where the code attempts to load tokenizer and image processor assets directly from a hard‑coded Hugging Face model reference instead of the locally deployed tokenizer path. This typically manifests as: Model startup failures Tokenizer / processor load errors Inconsistent behavior when running in offline environments To fix no configuration changes are required, copy and apply the provided patch on the board: root@imx95evk:~# chmod a+x apply_qwenvl_fix.sh root@imx95evk:~# sh apply_qwenvl_fix.sh remarks: please make sure the path in the script match your installation: PROD_FILE="/usr/share/eiq/aaf-connector/venv/lib/python3.13/site-packages/eiq_aaf_connector/llm_engines/QwenVL.py"
查看全文
Ara240 product image.jpg   Welcome to the Ara240 DNPU Training! This page provides access to training materials, presentations, demos, recordings, and supporting resources related to the Ara240 DNPU. While live Q&A support will be available during the training period, all content will remain accessible for future reference and self-paced learning. Required Hardware FRDM i.MX 95 Pro FRDM i.MX 8M Plus Ara240 DNPU Ara240 16GB M.2 Module microSD >= 64GB storage USB-C debug cable Internet (Ethernet) HDMI Monitor 100 W power supply (Anker Charger is recommended) USB mouse USB keyword 1080p USB Camera Instructions Step1. Watch introduction DNPU Training Introduction Step2. Check the Hardware and Software Pre-requisites Getting Started Guide with FRDM-IMX8MPLUS Step3. Run the rest of the Software demo packages After completing the pre-work, each lab has its own guide document and a video guide you can use as support material in case you have any question at any step: Lab1: Running a GStreamer Pipeline for 8 Video Streams with YOLOv8n on Ara240 DNPU Ara Vision Multi-Stream YOLOv8 Object Detection Lab2: Running Unimodal Large Language Models on Ara240 DNPU LLM Edge Studio Lab3: Interacting with Vision-Language Models on Ara240 DNPU VLM Edge Studio Lab4: Enabling REST-Based LLM and VLM Inference on Ara240 DNPU eIQ AAF Connector Additional Resources Take advantage of the resources below to deepen your knowledge and support your development efforts: Ara Software Development Kit (ARA SDK) Ara240 DNPU Six Pack Ara240 Discrete Neural Processing Unit (DNPU) Ara240 16GB M.2 Module FRDM i.MX 95 Pro FRDM i.MX 8M Plus  
查看全文
Introduction DNPU Training   Explore the evolution of AI at the edge, from perception AI and generative AI to the emerging era of Agentic AI. This session introduces NXP’s discrete NPU strategy and examines how neural networks, transformer models, and AI agents enable intelligent decision-making for industrial, healthcare, and automation applications. Participants will gain an understanding of the technologies driving the next generation of intelligent edge systems.
查看全文
Applies to: LLM / VLM Edge Studio Go Point Demo Workaround: Update demos via deb package In the current BSP release, users may encounter a runtime failure when the requesting inference metrics after running an inference in the LLM / VLM Edge Studio demo, as a result, metrics are not displayed at all. This issue is caused by a change in the metrics response format from the AAF Connector, which is not compatible with the current demo version.  To fix, update the demo by installed the patched Debian package attached to this thread.  - Download and copy deb packages to target board:  scp vlm-edge-studio_1.0.1.deb [email protected]: scp llm-edge-studio_2.0.1.deb [email protected]: - Overwrite the demo installation: dpkg -i --force-overwrite vlm-edge-studio_1.0.1.deb dpkg -i --force-overwrite llm-edge-studio_2.0.1.deb BR,
查看全文
This article provides you with general guidelines that apply for All Ara-2 Lab SW packages. Follow the steps below to download, prepare, and execute each lab successfully. 1. Download the Lab Package   All lab packages are hosted in the Ara2‑SW‑Packages v1.3.0 location. After opening the shared link: Navigate to corresponding Package folder Download all contents of that folder to your local machine Ensure the folder structure remains intact 2. Important Files Inside the Package   Each package includes two key HTML files: ️ INSTALL.html Provides step‑by‑step instructions to install prerequisites and prepare your environment. README.html Contains details about the lab scenario, execution steps, and additional notes. Important: These HTML files must be downloaded and opened locally. Opening them directly from the WorkDrive browser will cause them to load incorrectly. Once downloaded, simply double‑click to open them in your browser — they are fully self‑contained and easy to follow. 3. Running the Lab   After completing the installation steps in INSTALL.html: Review the scenario and steps in README.html Execute the lab tasks at your own pace Return to the forum to share results, ask questions, or support others! 4. Watch the Walkthrough Video   A video file is included in each package. This video walks you through the same steps described in INSTALL.html and README.html, providing a visual guide to installation, setup, and execution. You can use the video as: A companion guide while following the HTML instructions A quick overview before starting the lab A reference if you prefer visual, step‑by‑step walkthroughs    
查看全文
Watch Technical Overview Hands-On Training
查看全文