what these lines mean in .lcf file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what these lines mean in .lcf file

2,898 Views
doom
Contributor I
Here is my .lcf file and someting puzzling me...

# Sample Linker Command File for CodeWarrior for ColdFire


# Memory ranges

MEMORY {
vectorrom (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000420
code (RX) : ORIGIN = 0x00000500, LENGTH = 0x0001Fae0

my (RX) : ORIGIN = 0x0001fae0, LENGTH = 0x00000100

vectorram (RWX) : ORIGIN = 0x20000000, LENGTH = 0x00000400
userram (RWX) : ORIGIN = 0x20000400, LENGTH = 0x00007c00
}

SECTIONS {

# Heap and Stack sizes definition
___heap_size = 0x1000;
___stack_size = 0x1000;



# MCF5213 Derivative Memory map definitions from linker command files:
# __IPSBAR, __RAMBAR, __RAMBAR_SIZE, __FLASHBAR, __FLASHBAR_SIZE linker
# symbols must be defined in the linker command file.

# Memory Mapped Registers (IPSBAR= 0x40000000)
___IPSBAR = 0x40000000;

# 32 Kbytes Internal SRAM
___RAMBAR = 0x20000000;
___RAMBAR_SIZE = 0x00008000;

# 256 KByte Internal Flash Memory
___FLASHBAR = 0x00000000;
___FLASHBAR_SIZE = 0x00040000;

.userram : {} > userram
.code : {} > code
.vectorram : {} > vectorram
.vectorrom : {} > vectorrom


.absd:
{

*(.MacAddr)
= ALIGN (0x4);
} > my
.vectors
{
mcf5xxx_vectors.s (.text)
. = ALIGN (0x4);
} >> vectorrom

.text :
{
*(.text)
. = ALIGN (0x4);


*(.rodata)
. = ALIGN (0x4);


___ROM_AT = .;
___DATA_ROM = .;
} >> code
.data : AT(___ROM_AT)
{
___DATA_RAM = .;
. = ALIGN(0x4);
*(.exception)
. = ALIGN(0x4);
__exception_table_start__ = .;
EXCEPTION
__exception_table_end__ = .;

___sinit__ = .;
STATICINIT
__START_DATA = .;

*(.data)
. = ALIGN (0x4);
__END_DATA = .;

__START_SDATA = .;
*(.sdata)
. = ALIGN (0x4);
__END_SDATA = .;

___DATA_END = .;
__SDA_BASE = .;
. = ALIGN (0x4);
} >> userram

.bss :
{
___BSS_START = .;
__START_SBSS = .;
*(.sbss)
. = ALIGN (0x4);
*(SCOMMON)
__END_SBSS = .;

__START_BSS = .;
*(.bss)
. = ALIGN (0x4);
*(COMMON)
__END_BSS = .;
___BSS_END = .;

. = ALIGN(0x4);
} >> userram

.custom :
{
___HEAP_START = .;
___heap_addr = ___HEAP_START;
___HEAP_END = ___HEAP_START + ___heap_size;
___SP_END = ___HEAP_END;
___SP_INIT = ___SP_END + ___stack_size;

. = ALIGN (0x4);
} >> userram

___VECTOR_RAM = ADDR(.vectorram);

__SP_INIT = ___SP_INIT;

_romp_at = ___ROM_AT + SIZEOF(.data);
.romp : AT(_romp_at)
{
__S_romp = _romp_at;
WRITEW(___ROM_AT);
WRITEW(ADDR(.data));
WRITEW(SIZEOF(.data));
WRITEW(0);
WRITEW(0);
WRITEW(0);
}

}


what these lines mean?
.userram : {} > userram
.code : {} > code
.vectorram : {} > vectorram
.vectorrom : {} > vectorrom


Can I delete them?
I also define a section myself and not use command like that and it is ok!
why? What is the different between my section and others?
Can anyone explain it?

doom
Labels (1)
0 Kudos
Reply
4 Replies

1,492 Views
CrasyCat
Specialist III

Hello

 

The lines

.userram : {} > userram
.code : {} > code
.vectorram : {} > vectorram
.vectorrom : {} > vectorrom

 

Indicates  that you are placing the section .userram from your application in the memory area userram, section .code into memory area code, section .vectorram in memory area vectorram and section vectorrom in section vectorrom.

 

If you are sure these sections are not used at all in your application, you can remove the lines from the .lcf file.

I would try to link the application as it is and check the generated .map file to make sure the sections really do not exist in your final application.

 

CrasyCat

0 Kudos
Reply

1,492 Views
EdProulx
Contributor I

My issue is that I would like to load my application into flash at a specific address (my goal: eventually download a 2nd application to yet some other flash location, and when the system is reset, execute using this newly downloaded application).

 

In my .lcf link control file, I specify:

 

MEMORY {
   vectorrom   (RX)  : ORIGIN = 0x00002000, LENGTH = 0x00000400
   cfmprotrom  (RX)  : ORIGIN = 0x00002400, LENGTH = 0x00000020
   code        (RX)  : ORIGIN = 0x00002A00, LENGTH = 0x0003FB00
   vectorram   (RWX) : ORIGIN = 0x20000000, LENGTH = 0x00000400
   userram     (RWX) : ORIGIN = 0x20000400, LENGTH = 0x00007C00
}
 

This will load and launch my application in flash from 0x2A00. The vector table is located in 0x2000 which I verify via the debugger, data is valid. But the system crashes ("Exception name vector: Address Error")  if I "Run" it or attempt to step through the _startup entry routine.

 

If vectorrom is not at 0x00000000 then the system crashes - always. If the vectorrom is at the ZERO address, the system runs fine, entering the "code" as per its specification in the MEMORY section. So I can run code from anywhere in flash. But I need to have the vector table in flash also at a specific location in flash.

 

Any help to get me past this problem would be greatly appreciated.

0 Kudos
Reply

1,492 Views
PaoloRenzo
Contributor V

Seems like you're using an MCU

 

flashbar always always starts at zero after each reset, then will start to look for vector table at zero.

 

you're lucky to start debugging code since you're using the debugger, which fixes these values using cfg file. you will not be able to see anything in standalone mode

 

you can change flashbar at runtime, not at the beggining

 

in my opinion, i don't think it's necessary to change flashbar even at runtime, seems more useful for MPUs with external memory

 

have you seen the first two longwords at vector table? those point to starting address and SP initial value

 

does this make sense to you or i completely misunderstood your question?

0 Kudos
Reply

1,492 Views
EdProulx
Contributor I

Actually, it makes perfect sense. Not good sense, but perfect. In fact, it was only after I posted that I was reading the ColdFire MCF52259_CMRM reference manual, where in section "3.2.6 Vector Base Register (VBR)" it states:

 

 

The VBR contains the base address of the exception vector table in memory. To access the vector table,the displacement of an exception vector is added to the value in VBR. The lower 20 bits of the VBR are not implemented by ColdFire processors. They are assumed to be zero, forcing the table to be aligned on a 1 MByte boundary

 

 

Well, I have 512K of flash. So the vector table *MUST* reside at address 0x0, so it cannot be moved elsewhere.

 

Now that I understand this aspect more clearly, I have to consider other alternative solutions to reach my goal.

0 Kudos
Reply