upload uClinux on MCF5329

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

upload uClinux on MCF5329

ソリューションへジャンプ
2,395件の閲覧回数
DarioD
Contributor I

Hi!

    Where can I find a guide for install/use uClinux on my MCF5329?

    Can I manage its GPIOs easily? And how?

Thanks and best regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,543件の閲覧回数
obidon
Contributor III

You can install following the instructions included with the board support package. http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A9 If you are using Fedora 9 it installs with no problems. For Fedora 10 or 11 you may get an error about rpm-build. There is another thread relating to that. Since the 5329 is a non-MMU micro and there is no problem accessisng GPIOs. You can write or read them directly just like with a non-OS application.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,544件の閲覧回数
obidon
Contributor III

You can install following the instructions included with the board support package. http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A9 If you are using Fedora 9 it installs with no problems. For Fedora 10 or 11 you may get an error about rpm-build. There is another thread relating to that. Since the 5329 is a non-MMU micro and there is no problem accessisng GPIOs. You can write or read them directly just like with a non-OS application.

0 件の賞賛
返信