uTaskerV1.3 to CodeWarrior Ecliplse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uTaskerV1.3 to CodeWarrior Ecliplse

2,183 Views
xuuurraa
Contributor II

Hi, 

I have an old firmware of uTasker V1.3, compiled in CodeWarrior Classic, now, I would like to implement the code in the new CodeWarrior and Windows10.

Can anyone tell me how can I do it???

I'm working in old hardware design with MCF52212 xip, and this only read a keyboard and send via USB to the PC. 

0 Kudos
Reply
3 Replies

1,969 Views
TomE
Specialist II

Which version of "CW Classic"? If it is 7.1 or prior, then you've got a problem.

CW changed the ABI in 7.2, breaking pretty much all previous example code (that used any assembly). If your "CW Classic" is 7.2 or after then it should be OK. If prior, then read this first and follow the links:

https://community.nxp.com/message/401840

Options are:

1 - "Archive the old build environment" (old OS, old CW, old uTasker, old code) and run it in a VM on your new computer,

2 - Update to latest uTasker (it shouldn't be all that different to the user code), or

3 - Manually rewrite every assembly function in the old uTasker code and every C source that depends on the ABI. This would be very difficult.

If this is a "Hobby" or "Educational" project then you can license uTasker for free. If it is a commercial project, then the cost of uTasker is about 2 to 4 DAYS worth of what a Programmer earns, so if it gets the job done earlier it has paid for itself.

Tom

0 Kudos
Reply

1,969 Views
xuuurraa
Contributor II

Thanks, now i have the new uTasker and I´m trying to update the old code.

Regards, Xavi

0 Kudos
Reply

1,969 Views
miduo
NXP Employee
NXP Employee

Hi,

Does this help: How to Send USB HID Keyboard Keystrokes to PC using uTasker?? 

If this no help, I'd suggest you look on the uTasker site.

0 Kudos
Reply