problem write the tcpip stack interniche with the web server in the flash mem of the MCF52235EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem write the tcpip stack interniche with the web server in the flash mem of the MCF52235EVB

2,118件の閲覧回数
fjoli
Contributor I
Hello
 
I'm trying to write the tcp/ip stack from interniche with the web server in the internal flash memory of the MCF52235EVB but it doesn't work. So I can't acces to the web server.
I work with CodeWarrior v7.0 and I use the flash programmer.
I had erased what was on the flash memory so the web server which was on the board when I got it isn't already in.
Is it posible to recuperate the precedent program which was in the flash memory somewhere ?
 
Thanks
Fabien
ラベル(1)
0 件の賞賛
返信
1 返信

1,250件の閲覧回数
RickN
Contributor I
Hi,
 
   Take a look at the information on the following link:
 
 
   I see the MCF52233 demo is provided here, and it may also run on the MCF52235.
 
  
    Thanks,
 
          Rick
0 件の賞賛
返信