problem with MSL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with MSL

2,174 Views
LPs1978
Contributor III

Hi all,

   I'm having trouble with my project where I ported the FreeRTOS OS on a MCF52221.

I need to use the standard sprintf functio, nut if I use a standard complete MSL (C_4i_CF_StdABI_MSL.a) the project goes in Cpu_Interrupt because of some error accours.

 

The solution i fount out is to use the small MSL library (C_4i_CF_StdABI_SZ_MSL.a) as the guide saidformy processor. This means that a lot of functions like ato() atof() don't work. Another thing is that sprintf function has not complete functionality, like 0 padding.

 

What I'm asking is: is there some option to use a complete MSL liibrary with MCF52221 or is mandatory to use the small one?

 

regards

Labels (1)
0 Kudos
Reply
2 Replies

1,437 Views
vier_kuifjes
Senior Contributor I
0 Kudos
Reply

1,437 Views
LPs1978
Contributor III

I helpful, I read it before to post my question.

 

What I need is to know if the problem that I have with standard MSL library is a "standard problem" or is somethoing in my appplication that make sthe sprintf working wrong.

 

 

0 Kudos
Reply