problem with MSL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with MSL

2,199件の閲覧回数
LPs1978
Contributor III

Hi all,

   I'm having trouble with my project where I ported the FreeRTOS OS on a MCF52221.

I need to use the standard sprintf functio, nut if I use a standard complete MSL (C_4i_CF_StdABI_MSL.a) the project goes in Cpu_Interrupt because of some error accours.

 

The solution i fount out is to use the small MSL library (C_4i_CF_StdABI_SZ_MSL.a) as the guide saidformy processor. This means that a lot of functions like ato() atof() don't work. Another thing is that sprintf function has not complete functionality, like 0 padding.

 

What I'm asking is: is there some option to use a complete MSL liibrary with MCF52221 or is mandatory to use the small one?

 

regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,462件の閲覧回数
vier_kuifjes
Senior Contributor I
0 件の賞賛
返信

1,462件の閲覧回数
LPs1978
Contributor III

I helpful, I read it before to post my question.

 

What I need is to know if the problem that I have with standard MSL library is a "standard problem" or is somethoing in my appplication that make sthe sprintf working wrong.

 

 

0 件の賞賛
返信