problem ethernet switch vs hub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem ethernet switch vs hub

2,744件の閲覧回数
VeronicaFNX
Contributor I
Hello,
 
I have made with coldfire a network with Ethernet (without using protocols). I connect several cards by means of switch or through hub and the network works well. But I have switch industrialist and nothing works. They have said to me that it can be a problem with the levels. It can be that? as I can solve the problem. I have a M52233demo
 
Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,711件の閲覧回数
mjbcswitzerland
Specialist V
Hi

Please check out the following forum posting. It may explain the problem that you are having.

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=363&query.id=8492#M36...

Regards

Mark


0 件の賞賛
返信

1,711件の閲覧回数
VeronicaFNX
Contributor I
Thanks Mark, you are very useful. :smileywink:
0 件の賞賛
返信