no MQX in codewarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

no MQX in codewarrior

2,852 次查看
andylong_2024
Contributor III

I have installed MQX 4.2(location : D:\066-Program-DO-NOT-DELETE\MQX RTOS)

and codewarrior Version: 11.1 (location :D:\066-Program-DO-NOT-DELETE\CW MCU v11.1)in my PC,

but I can not build the project with MQX,

even I want to set up a project with MQX,  lick file->new->,no MQX to see, only could see linux or uclinux...

could you help me ?

or tell me the link to see the method for setting up codewarrior and MQX development platform.

the MCU is MCF54415

thank you very much.

0 项奖励
回复
2 回复数

2,260 次查看
marcomello95
Contributor I

I'm with the same problem, but in CW 10.7. Coul you find any solution ?

0 项奖励
回复

2,827 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

The MCF54415 does not support MQX4.2, take in mind  that this processor is out of support and take care of your codewarrior version.

 

Regards