[mcf5484czp200] How do i map the alphanumeric pin data in BSDL file of mcf5484czp200 to numeric pin data of same uC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[mcf5484czp200] How do i map the alphanumeric pin data in BSDL file of mcf5484czp200 to numeric pin data of same uC?

972 Views
mohit_kumar
Contributor I

I am using Coldfire uC with reference Manufacturer No. MCF5484CZP200. The Pins of this uC are alphanumeric in BSDL file found in the internet.
For Boundary scanning purpose,I have to map this BSDL file to other file which contains only numeric pin numbers for the same uC. Now there is No sequential mapping of numeric and alphanumeric numbers & no logical pattern is seen in the mapping. 
E.g. - A2 pin(in bsdl) mapped to 152 pin(in netlist)
A3 pin(in bsdl) mapped to 174 pin(in netlist)
D2 pin(in bsdl) mapped to 175 pin(in netlist)
N2 pin(in bsdl) mapped to 179 pin(in netlist) etc.

Manually mapping is very cumbersome & time taking since many fpga and IC are used and each is having 600+ pins.

Is there any method to map numeric and alphanumeric numbers?

0 Kudos
Reply
1 Reply

854 Views
miduo
NXP Employee
NXP Employee

Hello,

Yes, I understood this situation. But sorry we do not provide any method & tool to map numeric and alphanumeric numbers besides the BSDL file itself.

0 Kudos
Reply