mcf5225x  ADC pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcf5225x  ADC pins

1,153件の閲覧回数
KriendDay
Contributor I

Hi,

 

I've been loading the example ADC program that come with MQX 3.8.1 on to my m52259demo board.  It's working on screen (via serial).  However,  I'm having a tough time actually sampling anything.  I don't know how it was set up.  Primarily, I understand that your ref voltage pins are based on what you write to the CAL (power reference) register.  I have tried connecting AN2 to the board's 3.3v output and AN6 to the board's ground and to the supply's negative terminal.  I then connect AN0 to the supply's positive terminal.  Is this the correct way of setting it up.  There's no changes when I vary the DC power supply's voltage.

 

On the other hand, I can't even touch the Vrl and Vhl pins.  They come straight off the microprocessor.

 

Can anyone with experience with the ADC program that comes with this MQX help?  Cheers

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)