mcf5213 IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcf5213 IDE

2,865件の閲覧回数
cgan5
Contributor I

Hello, 

I need to get the compiler for microprocessor ColdFire MCF5213. And this compiler should be able to run with Window 7 and Window 10.

Do you have any recommendation.

I know that Code Warrior Development Studio is able to do the job. However, it state in the website that it ran on Window 2000 or XP OS.

Thank you!

Best Regards,

Darren

0 件の賞賛
返信
5 返答(返信)

2,757件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below CodeWarrior IDE software for ColdFire MCF5213.

CodeWarrior® for MCUs (Eclipse IDE) - ColdFire®, 56800/E DSC, Kinetis®, Qorivva® 56xx, RS08/S08, S12...

pastedImage_1.png

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,757件の閲覧回数
cgan5
Contributor I

Hello Mike,

I installed the CodeWarrior IDE v11.1 successfully.

However, when I tried to Import the mcp project (a legacy one with target processor MCF5213), the IDE complained about "This toolchain is not supported for this target". 

Please see image below.

Unsupported ToolChain.JPG

Do you know where can I get this toolchain?

Thank you!

Best Regards,

Darren

0 件の賞賛
返信

2,757件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Darren,

There is an application note AN4104 about converting ColdFire legacy CodeWarrior project to CodeWarrior for MCU V10.0.

While, If this application note doesn't work on your site.

I would recommend use CW for MCU V11.1 create a new project based on MCF5213 chip and porting related codes to this project.

Thank you for the attention.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,757件の閲覧回数
cgan5
Contributor I

Thank you Mike for the information.

I am trying out both CW V11.1 as well as CW Classic IDE V6.3 for these legacy code.

However, with Classic IDE V6.3, I am missing the support folder "E68K_Support\Runtime\Runtime_68K\(Common_Source)"...

Is this folder available in Classic IDE V6.4?

I had been trying to locate the link to download this V6.4 IDE.....

Do you know where can I get one?

Thank you!

Best Regards,

Darren

0 件の賞賛
返信

2,757件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Darren,

I couldn't find the CodeWarrior Classic IDE v6.4 download resource.

I can only find CW Classic for ColdFire V7.2 download link at here.

Sorry for that.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信