mc52233demo: help flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc52233demo: help flashing

2,426 次查看
sk7499
Contributor I
hello i have a mc52233demo microcontroller im trying to flash the memory and i get a connection error the codewarrior application states that PEMicroProtocolPlugin not detected.  The thing is i connected the board via usb and ethernet i can ping the device and i get the standard web page at ip-192.168.1.4 the lights are on so there is conectivity but i cant flash the memory.  I have installed code warrior 5.7, 6.2 and 6.3 and all of them have the same issue does anyone have the same problem.  Or does anyone know how to fix this issue.
 
(Alban changed useless subject)

Message Edited by Alban on 2006-09-13 11:38 AM

标签 (1)
0 项奖励
回复
1 回复

1,485 次查看
juan_mendoza
NXP Employee
NXP Employee
There are a couple things you can check.  First my assumptions:
 
1. Using P&E USB ColdFire Multilink
2. Using example software.
 
Check the following:
 
1.  Any other versions of Codewarrior installed?
2. CFFlasher and Codewarrior not running at the same time.
3. In your project settings under Debugger-> Remote Debugging in the Connection drop down box check to make sure USB is selected.
4.  Try reinstalling the drivers for the P&E Multilink from www.pemicro.com. 
 
I hope this helps :smileyhappy:.
0 项奖励
回复