m52233DEMo and WDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

m52233DEMo and WDT

1,930 Views
WOLF
Contributor I
Can anyone explain how to enable and use the WDT on a the M52233DEMO?
 
Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,156 Views
mjbcswitzerland
Specialist V
Hi Wolf

The M52233 has a core watchdog timer which can be disabled (writing 0 to CWCR) or programmed to generate an interrupt when it times out. Eg (with 2s timeout at 60MHz PLL):

 #define WATCHDOG_2_SEC    0x30                                         // about 2 seconds at 60MHz bus
CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF); // activate watchdog
fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout); // enter watchdog interruot
IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);
IC_IMRL_0 &= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);  // enable wacthdog interrupt

Note that the watchdog can not generate a reset directly so the interrupt is set to highest level, non-maskable so that it has highest chance of being able to operate.

To generate a reset when the watchdog fires, and its interrupt (_sw_wdog_timeout()) is called, the following can be performed:
    RESET_RCR = SOFT_RST;                                                // command a soft reset of the board

To stop the watchdog from firing it must be regularly reset by using the following feed sequence:
        CWSR = 0x55;                                                     // retrigger the software watchdog
        CWSR = 0xaa;                                                     // using this two byte sequence

Note that the watchdog should not be enabled when debugging since it fires when single stepping and causes loss of debugger control.

There are several other discussions about the pros and cons of the watchdog timer in the forum (eg. http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=2759&query.id=49225#M...

Note that other parts, like the M52213 include a second watchdog called the Background Watchdog Timer, which is capable of directly generating a warm reset on underflow - this allows more reliable protection against SW errors.

Regards

Mark

www.uTasker.com



0 Kudos
Reply