How to connect a Wlfson codec WM8750 to MCF5251 CPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect a Wlfson codec WM8750 to MCF5251 CPU

2,770 次查看
Varindra
Contributor I
Hi,
         We have to interface the WM8750 codec to MCF5251, this CPU has 3 no. I2S
Controller - 1st Interface is I/O, 2nd interface is only Out & 3rd
interface is only In. We are not sure about the status about the  DAC &
ADC (Word Clock) in the WM8750 codec, i.e. whether there are two seperate clock
required while bit clock can be the same. Presently we have taken word clock
from 1st interface & 2nd interface, bit clock from the 1st interface and
DIN & DOUT from the 1st interface of the MCF5251 to WM8750 codec connection. Is
it ok ? or else how we can connect.

WM8750 has a common bit clock, ADCLRC & DACLRC (i.e. seperate word clock for ADC &
DAC inside), DIN, DOUT.

Thanks & Regards,
Varindra
标签 (1)
0 项奖励
回复
2 回复数

1,510 次查看
ShenLi
Contributor I
Hello, Varindra
I am doing a M5253 design with WM8731, I think it might give you some help. Please check the attachment. I have successfully run  a simple loop back (from earmic to earphone) through WM8731+ MCF5253.
0 项奖励
回复

1,510 次查看
Varindra
Contributor I
Hi Shen,
                  Thanks for the reference.

Thanks & Regards,
Varindra
0 项奖励
回复