lamp dimmer system advice

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lamp dimmer system advice

3,556 Views
airswit
Contributor III
Hi, I am working on my design project to graduate college, and am making a lamp dimmer controller. I was wondering the best way to use a 5213 to accomplish this. I am thinking of hooking a zero detector circuit to an interrupt pin, which in turn will reset the PWM timers. The lamp dimmer drivers (opto-isolated triac drivers) will be hooked (indirectly) to the PWM output pins. I would like to be able to control about 8 loads, and am just wondering if there is a better way then to just use the PWM's. Also, can anybody point me in the direction of a zero crossing detector for 120Vac? Any help appreciated!
Labels (1)
0 Kudos
Reply
1 Reply

1,933 Views
tequila
Contributor I
The Zero Crossing Detector depends on the power supply (transformer mb?) you are to use.
 
Anyway, assuming you are only programming the dimmer, Isn't a Coldfire device huge for the application?. MB a 8/16 Bit Microcontroller would be a better choice.
 
Cheers:smileyhappy:
0 Kudos
Reply