lamp dimmer system advice

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lamp dimmer system advice

3,489件の閲覧回数
airswit
Contributor III
Hi, I am working on my design project to graduate college, and am making a lamp dimmer controller. I was wondering the best way to use a 5213 to accomplish this. I am thinking of hooking a zero detector circuit to an interrupt pin, which in turn will reset the PWM timers. The lamp dimmer drivers (opto-isolated triac drivers) will be hooked (indirectly) to the PWM output pins. I would like to be able to control about 8 loads, and am just wondering if there is a better way then to just use the PWM's. Also, can anybody point me in the direction of a zero crossing detector for 120Vac? Any help appreciated!
ラベル(1)
0 件の賞賛
返信
1 返信

1,866件の閲覧回数
tequila
Contributor I
The Zero Crossing Detector depends on the power supply (transformer mb?) you are to use.
 
Anyway, assuming you are only programming the dimmer, Isn't a Coldfire device huge for the application?. MB a 8/16 Bit Microcontroller would be a better choice.
 
Cheers:smileyhappy:
0 件の賞賛
返信