interfacing sdcard using qspi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interfacing sdcard using qspi

4,645件の閲覧回数
yuvi
Contributor I
Hi,
I am using MCF52223EVB & trying to connect the sd card to QSPI bus.
But can't seem to get it working . I tried to search the forum but couldn't
get much help. Please can someone who has succesfully done this
before guide me in the right direction.
 
thanks
yuvi
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,134件の閲覧回数
RichTestardi
Senior Contributor II
Have you seen this?
 
 
Also, can you tell us what, specifically, doesn't work and how?
 
And what software you are using?
 
If it helps to see my qspi driver, it is attached (ignore the 51jm128 code -- you want the 52221/52233 code).
 
-- Rich
 
 
0 件の賞賛
返信

3,134件の閲覧回数
stzari
Contributor III
Hi,

did you configure the GPIOs ?
Do you see any clock or data on the lines ?

stzari
0 件の賞賛
返信

3,134件の閲覧回数
yuvi
Contributor I
yes i have initialised GPIOs .
 
  MCF_GPIO_PQSPAR = ( MCF_GPIO_PQSPAR_DOUT_GPIO  
                                            | MCF_GPIO_PQSPAR_DIN_GPIO  
                                            | MCF_GPIO_PQSPAR_SCK_GPIO        
                                            | MCF_GPIO_PQSPAR_CS0_GPIO)
 
& no i can't detect any clock & data on the QSPI.
I have initialised GPIOs before setting up the QSPI registers(i believe thats the
correct ways to do it).
 
 
0 件の賞賛
返信

3,134件の閲覧回数
bkatt
Contributor IV


yuvi wrote:
yes i have initialised GPIOs .
 
  MCF_GPIO_PQSPAR = ( MCF_GPIO_PQSPAR_DOUT_GPIO  
                                            | MCF_GPIO_PQSPAR_DIN_GPIO  
                                            | MCF_GPIO_PQSPAR_SCK_GPIO        
                                            | MCF_GPIO_PQSPAR_CS0_GPIO)
 

You need something like:

      MCF_GPIO_PQSPAR = (0
        | MCF_GPIO_PQSPAR_CS3_CS3
        | MCF_GPIO_PQSPAR_CS2_CS2
        | MCF_GPIO_PQSPAR_CS1_CS1
        | MCF_GPIO_PQSPAR_CS0_CS0
        | MCF_GPIO_PQSPAR_SCK_SCK
        | MCF_GPIO_PQSPAR_DIN_DIN
        | MCF_GPIO_PQSPAR_DOUT_DOUT);

0 件の賞賛
返信

3,134件の閲覧回数
yuvi
Contributor I
Hi everyone,
thanks for your replies. i finally got it working. the problem was as indicated by bkatt the GPIO setting.
i was using qspi_cs3  for initialization which was already  configured for USB pull down. i connected
my sd card to cs0 & got it working .
but here arises a new question that all these GPIOs are mutually exclusive . what if i wish to connect 4
peripherals to qspi & also use USB then what do i need to do??
 
thnks again
0 件の賞賛
返信