how to continuously try to auto connect?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to continuously try to auto connect?

ソリューションへジャンプ
3,584件の閲覧回数
jonasb
Contributor I

hey I'm using the coldfire-lite tcp client. The board that I'm using is m52233DEMO.I can connect to the server this is working fine. But I wan't to know how to program my board to try continuously make a connection even if the server is not running.  But when I reset or shutdown the server or the board the board has to reconnect but that isn't working.

 

some information about the server: The server auto drops the connection when there is no reply of board the server knows this because the board is sending a keep_alive to the server. When there is no keep_alive send the server wait's for about 5s and then disconnect the board.

 

this is a part of code of my tcp_init

 

int freescale_tcp_init()
{   

    const char* loginname;
   
    semaphore                         = 0;
    flash_ffs_lockout                 = 0;
    emg_tcp_communication_socket     = INVALID_SOCKET;
   
    // Init message queue for MINI_TCP socket interface
    msring_init(&emg_tcp_msring, emg_tcp_msring_buf, sizeof(emg_tcp_msring_buf) / sizeof(emg_tcp_msring_buf[0]));

    // Init a socket structure with our Port Number
    emg_tcp_sin.sin_addr.s_addr     = (SERVER_IP);
    emg_tcp_sin.sin_port            = (PORT_NUMBER);

    emg_tcp_communication_socket    = m_socket();

    printf( "\nConnecting to target..." );
   

    //m_ioctl(emg_tcp_communication_socket, SO_NONBLOCK, NULL);    //make socket non blocking   


    e = m_connect(emg_tcp_communication_socket, &emg_tcp_sin, freescale_tcp_cmdcb );
   
   
   if ( e > 0 )
    {
        send_alive = 1;
        if( e == ECONNREFUSED )
        {
            printf( " - Cold Not Find Target, reset" );
            freescale_tcp_init();
                emg_tcp_communication_socket     = INVALID_SOCKET;
                m_close (emg_tcp_communication_socket);
                m_close (emg_tcp_server_socket);
        }
        else
            printf(" - error %d starting listen on emg TCP server\n", e);
            freescale_tcp_init();
                emg_tcp_communication_socket     = INVALID_SOCKET;
                m_close(emg_tcp_communication_socket);
                m_close(emg_tcp_server_socket);
 

          m_ioctl(emg_tcp_communication_socket, SO_NONBLOCK, NULL); //make socket non blocking   
   
    }

   
    if (e == 0)
    {
    emg_tcp_server_socket = emg_tcp_communication_socket;

    .....

ラベル(1)
0 件の賞賛
返信
1 解決策
2,310件の閲覧回数
vier_kuifjes
Senior Contributor I

The actual TCP fix is located in the file TCPAPI.C, which is buried in some folder in the Coldfire Lite project. To make things simple, I have attached the fixed version of that file to this message.

 

- Marc

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,310件の閲覧回数
jonasb
Contributor I

Thanks for the reply but i got still one error.

I made a loop. Then he says about 18 times "cold not find target, reset". Then he gives an error that there is no memory left. I was searching and i found he did an alloc. So he makes a reservation for some memory 18 times. I think i have to do something with free my memory. I found something like TCB_FREE. I tried somethings but i still get acces error. Does anyone can help me.

 

Thanx

Message Edited by jonasb on 2009-04-24 09:21 AM
0 件の賞賛
返信
2,310件の閲覧回数
jonasb
Contributor I
I hope this solve's the problem. But will it also try connecting after that the connection is lost (I mean when the server not properly disconnect) by example when the switch is down?
0 件の賞賛
返信
2,310件の閲覧回数
vier_kuifjes
Senior Contributor I

You set up the connection using the m_connect function. This function returns 0 when successful, and nonzero when it fails. It is up to the code to re-attempt to connect to the server. You will probably have to set up some kind of loop to do this...

 

I hope this is what you were asking?

0 件の賞賛
返信
2,311件の閲覧回数
vier_kuifjes
Senior Contributor I

The actual TCP fix is located in the file TCPAPI.C, which is buried in some folder in the Coldfire Lite project. To make things simple, I have attached the fixed version of that file to this message.

 

- Marc

 

0 件の賞賛
返信
2,310件の閲覧回数
vier_kuifjes
Senior Contributor I

Hello Jonas,

 

I too use the Coldfire Lite TCP client in my project. I have found that, when the TCP client tries to connect to a server that does not respond, it gets trapped in a wait loop that does not contain a timeout, so it will remain in this loop forever.

 

I have created a simple fix for this. You can find the fix in a document I posted here recently, see this thread:

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=6625

If you have any questions about this, just let me know!

 

- Marc

 

0 件の賞賛
返信
2,310件の閲覧回数
netra
Contributor IV

Hi Marc ,

I cannot find any solution in the given link by you . can you attach the solution in the reply itself.\

Thanks

Nisha

0 件の賞賛
返信