how MCF52232/MCF52236 replace MCF52233/52235?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how MCF52232/MCF52236 replace MCF52233/52235?

2,929 Views
gxd
Contributor I
I used MCF52233 and mcf52235 CPU for 2 years before.
 
MCF52233 system clock is 60MHz but new product is 50MHz.
 
For new product MCF52232/MCF52236 ,how to revise old source code in this change?
(the source code is based  on AN3455 ).
 
 
void
mcf5223_pll_init(void)
{
 /* The PLL pre-divider affects this!!!     no change!
  * Multiply 25Mhz reference crystal /CCHR by 12 to acheive system clock of 60Mhz
  */
 MCF_CLOCK_SYNCR = MCF_CLOCK_SYNCR_MFD(4) | MCF_CLOCK_SYNCR_CLKSRC| MCF_CLOCK_SYNCR_PLLMODE | MCF_CLOCK_SYNCR_PLLEN ;
 while (!(MCF_CLOCK_SYNSR & MCF_CLOCK_SYNSR_LOCK))
 {
 }
}
 
ADD:
MCF_CLOCK_CCHR=0x05;            ////            25MHz*12/6=50MHz
 
Whether need I do more thing except there?
 


Message Edited by gxd on 2008-10-13 08:25 AM
Labels (1)
0 Kudos
Reply
3 Replies

1,765 Views
gxd
Contributor I
I try it but the ethernet not pass.
 
i redefine SYSTEM_CLOCK  50 (mcf52235evb.h)
 
I find the problem in there:
 
void mcf5223_ePHY_init(void)
{
 uint32   myctr;      //generic counter variable
 uint16   mymrdata, mymwdata;     //temp variable for MII read/write data
   uint16  reg0, reg1, reg4;    //

 fec_mii_init((SYSTEM_CLOCK));
......
}
 
Need more ?
 
0 Kudos
Reply

1,765 Views
mjbcswitzerland
Specialist V
Hi

MCF_CLOCK_CCHR can not be changed - see the errata (this may however be corrected in newer chips).

For 60MHz operation MCF_CLOCK_SYNCR is set to 0x4007 ((25MHz / 5) * 12).
For 50MHz operation MCF_CLOCK_SYNCR is set to 0x3007 ((25MHz / 5) * 10).

Regards

Mark

www.uTasker.com



Message Edited by mjbcswitzerland on 2008-10-14 11:08 AM
0 Kudos
Reply

1,765 Views
MrBean
Contributor I


mjbcswitzerland wrote:
MCF_CLOCK_CCHR can not be changed - see the errata (this may however be corrected in newer chips).

In newer chips it indeed can be changed, very limited though.
See:
0 Kudos
Reply