getting started with MCF52233

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

getting started with MCF52233

Jump to solution
2,912 Views
ridges
Contributor I

Hello,

My name is Martin. I'm interesting in develop an application with MCF52233.

The application work's over tcp/ip network. I have some MCF52233 demo board. I'ud like to use then as client and the PC as server. My question is if there are any aplication note about this. I have the AN 3518. But i dont know if trere are any others application notes or information.

The project consist in read an tri axis accelerometer in demo board (client) and transmit to the PC (sever) over TCP/IP network. This projet is for the university.

well thanks to all and i'll waiting for your answer...

Martin

Labels (1)
0 Kudos
Reply
1 Solution
2,156 Views
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

View solution in original post

0 Kudos
Reply
2 Replies
2,157 Views
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

0 Kudos
Reply
2,156 Views
ridges
Contributor I

Hi,

 

Thank you very much for your recommendation. There is an example that is right for my application.

 

see you soon...

thanks again

Martin

0 Kudos
Reply