float to string

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

float to string

6,923 次查看
icarus31
Contributor III

Hi,

 

I have an issue to convert a float to a string with the Coldfire MCF52259. Here what I am trying to do:

 

char str[10];

float fval = 1201 / 10;

sprintf (str, "%3.1f\n", fval);

 

The debugger shows that fval is 120.100. This is what I expect to see. But "str" is not set correctly. If I do the same thing with an integer, there is no problem:

 

char str[10];

int val = 1201

sprintf (str, "%d\n", val);

 

 

What I am doing wrong?

 

Thanks in advance

标签 (1)
0 项奖励
回复
11 回复数

6,222 次查看
vier_kuifjes
Senior Contributor I

This thread may give you a hint for a solution:

https://community.freescale.com/thread/46585

0 项奖励
回复

6,222 次查看
scifi
Senior Contributor I

icarus31 wrote:

 

float fval = 1201 / 10;

... 

The debugger shows that fval is 120.100.


That's odd. This code should initialize fval with 120.0. I wonder if you edited the code before posting it. Maybe there are other significant differences?


icarus31 wrote:

 

sprintf (str, "%3.1f\n", fval);


Perhaps you meant "%5.1f"? Or simply "%.1f"?


icarus31 wrote:

 

But "str" is not set correctly.


 What's the contents of str?

0 项奖励
回复

6,222 次查看
icarus31
Contributor III

SciFi,

 

I should say "float fval = (float) 1201/10;"  I did not copy paste the code because I was working on another computer.

 

The "%3.1f" was basically make sure it will be 3 digits before the dot and 1 digit after it. So, it should print 120.1. The "%5.1f" or "%.1f", for that particular case will have the same result as what I wrote.

 

The "str" variable was set to :

 

str[0] = 'f'

str[0] = '\x00'

str[1] = '\x91'

str[2] = '\x9C'

str[3] = '\x00'

str[4] = '\x00'

str[5] = '\x00'

str[6] = '\x00'

str[7] = '\x00'

str[8] = '\x00'

 

 

0 项奖励
回复

6,222 次查看
scifi
Senior Contributor I

icarus31 wrote:

The "%3.1f" was basically make sure it will be 3 digits before the dot and 1 digit after it. 


So I figured. But that's not what it does. Look up format specifier reference.


icarus31 wrote:

The "str" variable was set to :

 

str[0] = 'f'

str[0] = '\x00'

str[1] = '\x91'

str[2] = '\x9C'

str[3] = '\x00'

str[4] = '\x00'

str[5] = '\x00'

str[6] = '\x00'

str[7] = '\x00'

str[8] = '\x00' 


 This appears to support BugMan's suggestion.

 

0 项奖励
回复

6,222 次查看
TomE
Specialist II

For those browsing this quickly and wanting to know why it printed what it did:

 

scifi wrote:

> icarus31 wrote:

> > The "str" variable was set to :

> >

> > str[0] = 'f'

> > str[0] = '\x00'

> >

> > "%3.1f"

> This appears to support BugMan's suggestion.

 

That was because the limited library scanned the print string, got to the "f", wasn't built for floats and thus converted "%f" to "f" in the buffer.

 

Tom

 

0 项奖励
回复

6,222 次查看
Nouchi
Senior Contributor II

Hello,

 

If I can give an advice, if you can, you'd better switch to CW7.2.2, because there's big improvement between CW7.1 and CW7.2.

If you keep CW7.1, if I remember, you have to rebuild libraries to enable printf floating point support.

0 项奖励
回复

6,222 次查看
icarus31
Contributor III

Sorry for the delay. I did not try anything yet, but I will once I come back to that project.

 

I will keep you posted

 

Thanks all!

0 项奖励
回复

6,222 次查看
Nouchi
Senior Contributor II

Hi,

 

If you use CW7.2, by librarian item, I meant Edit->"YourProject" Settings->Linker->Librarian.

You will find the same in CW10 : Project->Properties->C/C++ Build->Settings->tools settings->Librarian

 

Regards,

Emmanuel

0 项奖励
回复

6,222 次查看
icarus31
Contributor III

This is interresting, my version of CW 7.1.2 does not have the "Librarian" section under "Linker". I have "ColdFire Processor" and "Global Optimizations"

0 项奖励
回复

6,222 次查看
Nouchi
Senior Contributor II

Hello,

 

 

Your syntax seems to be right, did you check linker options?

You have to select int_FP option for print formatter in Librarian item, it could be the problem.

 

regards,

Emmanuel

0 项奖励
回复

6,222 次查看
icarus31
Contributor III

BugMan (Emmanuel),

 

Does the "Librarian item" is something is set in CodeWarrior? Is it in "Edit -> Int Flash Debug Settings" menu?

 

0 项奖励
回复