flas programing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flas programing

4,280 Views
fire
Contributor I
Hi,
  how to do flash programing on coldfire.
I tried and tired with the procedure given by them.
i don't where i went rong.
Please guide me in this issue.
Thank you.
Labels (1)
0 Kudos
Reply
2 Replies

1,882 Views
fire
Contributor I

Hai,

Thanks for your responce.I want to do flash programing on EVB 5282 lite.

I want to program in internal flash. I tried with Flasher supplied by coldfire.

But it is not working.

Please give me some idea.

Thank you.

0 Kudos
Reply

1,882 Views
UK_CF_FAE
NXP Employee
NXP Employee

Hi Fire,

You want to do flash programming.

1) Do you  want to program a ColdFire device or EVB from inside CodeWarrior?

2) Do you want to use an internal flash ColdFire device and use the flash for non-volatile memory, so-called Flash-As-EEPROM???

1) is easy, either with the Flash Programmer inside CodeWarrior, or with the freeware CF Flasher utility on www.freescale.com.

Let us know.

Mark

0 Kudos
Reply