dBUG ROM for M5407C3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

dBUG ROM for M5407C3

2,312 次查看
DiTBho
Contributor I

Back to 1999, the M5407C3 board was shipped with one Am29PL160C (2MByte) Flash ROM.

The first 256K of the Flash contains ROM Monitor firmware, named "dBUG", which provides the user with debug interface, inline assembler and disassembly, program download, register and memory manipulation, and I/O control functions.

The rest of the Flash was available for the user.

My board was saved today from the hydraulic press, someone must have reprogrammed the whole Flash because the VxWorks bootloader is the only thing that appears on the serial and there is nothing else in it  

By chance does anyone have a copy of the have a copy of dBUG?

0 项奖励
回复
2 回复数

2,270 次查看
DiTBho
Contributor I

thanks!

0 项奖励
回复

2,276 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I don't have M5407C3 board dBUG firmware.

While, I have the source code of ColdFire dBUG.

Hope it could help.

Mike

0 项奖励
回复