dBUG ROM for M5407C3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dBUG ROM for M5407C3

2,274 Views
DiTBho
Contributor I

Back to 1999, the M5407C3 board was shipped with one Am29PL160C (2MByte) Flash ROM.

The first 256K of the Flash contains ROM Monitor firmware, named "dBUG", which provides the user with debug interface, inline assembler and disassembly, program download, register and memory manipulation, and I/O control functions.

The rest of the Flash was available for the user.

My board was saved today from the hydraulic press, someone must have reprogrammed the whole Flash because the VxWorks bootloader is the only thing that appears on the serial and there is nothing else in it  

By chance does anyone have a copy of the have a copy of dBUG?

0 Kudos
Reply
2 Replies

2,232 Views
DiTBho
Contributor I

thanks!

0 Kudos
Reply

2,238 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I don't have M5407C3 board dBUG firmware.

While, I have the source code of ColdFire dBUG.

Hope it could help.

Mike

0 Kudos
Reply