commissioning MCF5208

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

commissioning MCF5208

3,231件の閲覧回数
fevernova
Contributor I
Hi at all,
I developed a board with the MCF5208 referenced to the M5208 evaluation board.
First of all I want to check the electrical connection with boundary scan, but it doesn't work.
The process failed. Then I tried the "hello world", but BDM doesn't work. There is no connection to the BDM.
 
Here are some information:
- voltages 3,3V and 1,5 are good
- /RESET is high-level
- RCON is pulled-down to gnd
- DRAMSEL is pulled-up to 3,3V (using sdram)
- DSCLK_/TRST, /BKPT_TMS, TDI_DSI, TDO_DSO are pulled-up
- PSTCLK_TCLK is pulled-down
- JTAG_EN is low when using BDM and high when using JTAG
 
Certainly there are a lot of approaches, but I'm thankful for any hints.
 
Are there any ideas to solve the problem? thanks to you
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,784件の閲覧回数
JWW
Contributor V
fevernova,

Did you make any more progress?  I would suggest getting BDM to work first, then proceeding to test JTAG.

What tools are you using to talk to the BDM?

Can you share a piece of your schematics for review?

-JWW

0 件の賞賛
返信

1,784件の閲覧回数
fevernova
Contributor I
Hi,
 
because of non-disclosure it's not possible to publish the schematics.
 
I use the PEMicro BDM via parallel port and Codewarrior 5.7 as IDE.
 
I took the 5208EVB project and at the moment I modify some configuration, e.g. flash size, sdram config...
 
I can exclude a wrong connection to the pc because with a 5213 board it works fine.
 
The message is:"PEMICROProtocolPlugin. Can't connect to PEMicro via parallel port."
0 件の賞賛
返信

1,784件の閲覧回数
fevernova
Contributor I
hi,
 
I have the following behaviour on my own 5208 board.
 
The core is supported by a crystal reference of 16MHz. After a few seconds the crystal stops to swing and goes into static high level. The fb_clk first seconds f=83.33MHz) stops at the same time, which is clear to me.
 
The RCON is asserted during reset and the config data pins fits with my configuration.
 
Is this a hardware bug in my design or is this still a normal behaviour?
0 件の賞賛
返信