assembly statements do not compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

assembly statements do not compile

5,692 Views
Veter
Contributor I
Following assembly statements were compiled with DIAB compiler. Does anyone knows eqivalent instructions in CW for ColdFire compiler.
 
/* save all of the registers we are going to modify */
__asm push es ;/* ES will contain a modified data segment */
__asm push di;/* DI is the offset of the data to sum */
__asm push dx;/* DX is the sum */
__asm push cx;/*CX is first used for temporary storage, and then to hold the loop control variable */
__asm les di, link16BitDataPtr;/* Load the pointer into ES:di */
 __asm mov cx, di;/* Save the offset portion of the pointer before we modify it */
__asm shr di, 4;/* Shift the offset right by 4 */
__asm push es;/* Copy the segment (es) into dx */
__asm pop dx;
__asm add dx, di;/* Add in the shifted offset */
__asm push dx;/* Copy the updated segment back into es */
__asm pop es;
__asm mov di, cx;/* Load the old offset, and mask off everything except the last 4 bits */
__asm and di, 000fh;
 
I am using CodeWarrior Development Studio for ColdFire Architectures Version 6.3, Build 14.
Labels (1)
0 Kudos
Reply
7 Replies

2,875 Views
Alban
Senior Contributor II
Hello,

/* save all of the registers we are going to modify */
asm{
    push es ;/* ES will contain a modified data segment */
    push di;/* DI is the offset of the data to sum */
    push dx;/* DX is the sum */
    push cx;/*CX is first used for temporary storage, and then to hold the loop control variable */
    les di, link16BitDataPtr;/* Load the pointer into ES:di */
    mov cx, di;/* Save the offset portion of the pointer before we modify it */
    shr di, 4;/* Shift the offset right by 4 */
    push es;/* Copy the segment (es) into dx */
    pop dx;
    add dx, di;/* Add in the shifted offset */
    push dx;/* Copy the updated segment back into es */
    pop es;
    mov di, cx;/* Load the old offset, and mask off everything except the last 4 bits */
}


is the way to present ASM it on CodeWarrior, I believe. But I didn't check the code is ok as you said it was working on other compiler.

Cheers,
Alban.
0 Kudos
Reply

2,875 Views
mccPaul
Contributor I
Hi Veter,
 
Can you say what this code snippet is trying to do? It looks like the start of a memory copy routine, but it's hard to say without seeing the whole thing. If you can say what the function needs to do, what parameters it is called with and which Coldfire you are using we may be able to give you Coldfire equivalent code.
 
Do you also know the target CPU for the original code? It looks like Intel assembler for a 16-bit target. As the Coldfire family is 32-bit, the code to move or copy memory is simpler because there is no need for data segments and far pointers so you don't really want a literal translation.
 
Cheers,
 
Paul.
 
 
 
 
0 Kudos
Reply

2,875 Views
Veter
Contributor I
The assembly code is embedded into the function that calculates packet's checksum. The entire function's body is copied below. The target is MCF5307. The embedded __asm assembly statements that push and pop stack contents do not comile with CW for ColdFire compiler. I am looking for equivalent assembly code that is accepted by this compiler.
 
/*
 * tfPacketChecksum() Function Description
 * This function performs checksum on (IP, ICMP, IGMP, UDP and TCP)
 * packets. Note that we cannot assume that data is contiguous. We follow
 * the chain of ttPacket (using the pktNextPtr), and compute the checksum
 * on each contiguous data area. We try and unroll the loop as much as we can.
 * This version handles odd byte lengths in inner links, and odd linkDataPtr.
 *
 * Parameter       Description
 * packetPtr       Pointer to a ttPacket. packetPtr->pktLinkDataPtr
 *                 points to the data to be checksummed.
 * length          Length of data to be checksumed.
 * Returns
 * Value   Meaning
 * 16bit one's complement checksum
 */
#include <trtype.h>
tt16Bit tfPacketChecksum (ttPacketPtr packetPtr, ttPktLen totalDataLength)
{
   tt16BitPtr         link16BitDataPtr;
   tt32Bit            sum;
   ttPktLen           linkLength;
   tt16Bit            sum16;
   unsigned short int bigLoop;
   unsigned short int switchOffset;
   union
   {
       tt16Bit  oddWord;
       tt8Bit   oddChar[2];
   } oddByte16Bit;
   tt8Bit        sumByteSwapped;
   sum = 0UL;
   linkLength = (ttPktLen)0;
   sumByteSwapped = TM_8BIT_ZERO;
/* packetPtr is assumed to be non null */
   do
   {
/* Point to data in this link */
       link16BitDataPtr = (tt16BitPtr)packetPtr->pktLinkDataPtr;
/* Loop through scattered data */
       if (linkLength == (ttPktLen)0)
       {
           linkLength = packetPtr->pktLinkDataLength;
       }
       else
       {
/* previous link had odd byte length, store 2nd byte to make a word */
           oddByte16Bit.oddChar[1] = *((tt8BitPtr)link16BitDataPtr);
/* add to sum */
           sum = sum + oddByte16Bit.oddWord;
/* Update pointer, and length. Pointer now is on odd byte boundary */
           link16BitDataPtr = (tt16BitPtr)((tt8BitPtr)link16BitDataPtr + 1);
           linkLength = packetPtr->pktLinkDataLength - 1;
           totalDataLength--;
       }
       if (linkLength > totalDataLength)
       {
/* Do not span more than asked */
           linkLength = totalDataLength;
       }
/* left over data to be checksumed after this link */
       totalDataLength -= linkLength;
/* Move pointer to even byte boundary */
       if ((tm_is_odd(link16BitDataPtr)) && (linkLength != 0))
       {
/* save odd byte for later addition */
           oddByte16Bit.oddChar[0] = *((tt8BitPtr)link16BitDataPtr);
/* Update pointer, and length. Pointer now is on even byte boundary */
           link16BitDataPtr =
                              (tt16BitPtr)((tt8BitPtr)link16BitDataPtr + 1);
           linkLength--;
/* Byte swap the sum, to collect odd bytes with odd bytes */
           tm_byte_swap_sum(sum);
           sumByteSwapped = TM_8BIT_YES;
       }
/*
 * How many times we are going to have to go through the big loop. Each time
 * through the loop, we add in 64 more bytes.
 */
       bigLoop = (unsigned short)((linkLength + 63) >> 6);
/* How far to jump into the switch statement */
       switchOffset = (unsigned short)(linkLength % 64);
/*
 * We do a shift right after this if. The shift is there because we operate
 * on 16 bits at a time, so we divide the number of bytes by 2. However,
 * a shift right means we'll lose a remainder of 1, so we have to deal with
 * it here. We don't actually add the extra byte into the sum right now, but
 * we still have to decrement the loop control variable
 */
       if (switchOffset == 1)
       {
           bigLoop--;
       }
/* Divide switchOffset by 2 */
       switchOffset = switchOffset >> 1;
       tm_fold_sum(sum);
/*
 * Chances are, the linkLength isn't going to be evenly divisible by 64. Thus,
 * we do calculations on the remainder first, and then use an optimized
 * assembly loop to handle the majority of the packet. While it would in fact
 * be possible, as well as marginally faster, to handle ALL of the
 * checksumming in assembly, this part is left in C to make porting to your
 * (the customer's) platform easier. If you are a confident assembly
 * programmer, this switch can be incorporated into the rest of the loop
 * (Duff's Device is one example of how it can be done).
 */
       switch (switchOffset)
       {
           case 31:       sum += *(link16BitDataPtr+30);
           case 30:       sum += *(link16BitDataPtr+29);
           case 29:       sum += *(link16BitDataPtr+28);
           case 28:       sum += *(link16BitDataPtr+27);
           case 27:       sum += *(link16BitDataPtr+26);
           case 26:       sum += *(link16BitDataPtr+25);
           case 25:       sum += *(link16BitDataPtr+24);
           case 24:       sum += *(link16BitDataPtr+23);
           case 23:       sum += *(link16BitDataPtr+22);
           case 22:       sum += *(link16BitDataPtr+21);
           case 21:       sum += *(link16BitDataPtr+20);
           case 20:       sum += *(link16BitDataPtr+19);
           case 19:       sum += *(link16BitDataPtr+18);
           case 18:       sum += *(link16BitDataPtr+17);
           case 17:       sum += *(link16BitDataPtr+16);
           case 16:       sum += *(link16BitDataPtr+15);
           case 15:       sum += *(link16BitDataPtr+14);
           case 14:       sum += *(link16BitDataPtr+13);
           case 13:       sum += *(link16BitDataPtr+12);
           case 12:       sum += *(link16BitDataPtr+11);
           case 11:       sum += *(link16BitDataPtr+10);
           case 10:       sum += *(link16BitDataPtr+9);
           case 9:        sum += *(link16BitDataPtr+8);
           case 8:        sum += *(link16BitDataPtr+7);
           case 7:        sum += *(link16BitDataPtr+6);
           case 6:        sum += *(link16BitDataPtr+5);
           case 5:        sum += *(link16BitDataPtr+4);
           case 4:        sum += *(link16BitDataPtr+3);
           case 3:        sum += *(link16BitDataPtr+2);
           case 2:        sum += *(link16BitDataPtr+1);
           case 1:        sum += *(link16BitDataPtr);
/* Fold the sum back into 16 bits */
                          tm_add_carries_sum(sum);
/* Increment the pointer */
                          link16BitDataPtr += switchOffset;
/* Decrement the loop control variable */
                          bigLoop--;
       }
/* Put the sum into a 16 bit stack variable */
       sum16 = (tt16Bit)(sum&0xffffUL);
/* We have to save all of the registers we are going to modify */
/* ES will contain a modified data segment */
       __asm push es ;
       
/* DI is the offset of the data to sum */
       __asm push di;
/* DX is the sum */
       __asm push dx;
/*
 * CX is first used for temporary storage, and then to hold the loop control
 * variable
 */
       __asm push cx;
/* Load the pointer into ES:di */
       __asm les di, link16BitDataPtr;
/*
 * We need to normalize the pointer, because of the segment/offset memory
 * scheme x86 real-mode processors use. To do this, we shift offset right
 * by 4, and add it to the segment. That total is the new segment, and
 * the new offset is the lowest 4 bits of the old offset. Both the new and
 * old addresses point to the same location in memory, but with the new,
 * normalized pointer, we don't ever have to worry about a packet being
 * long enough to necessitate incrementing the segment. This optimization
 * saves us significant time in the loop itself.
 */
/* Save the offset portion of the pointer before we modify it */
       __asm mov cx, di;
/* Shift the offset right by 4 */
       __asm shr di, 4;
/* Copy the segment (es) into dx */
       __asm push es;
       __asm pop dx;
/* Add in the shifted offset */
       __asm add dx, di;
/* Copy the updated segment back into es */
       __asm push dx;
       __asm pop es;
/* Load the old offset, and mask off everything except the last 4 bits */
       __asm mov di, cx;
       __asm and di, 000fh;
/* Zero out DX */
       __asm xor dx, dx;
/* Clear the carry bit and load sum16 into DX */
       __asm add dx, sum16;
/* Load the counter into cx */
       __asm mov cx, bigLoop;
TL_CHECKSUM_LOOP_TOP:
/* or the counter with itself. If it's 0, jump out of the loop */
       __asm or cx, cx;
       __asm jne TL_CHECKSUM_LOOP_CONTINUE;
       __asm jmp TL_CHECKSUM_LOOP_END;
/* decrement the counter by 1 */
TL_CHECKSUM_LOOP_CONTINUE:
       __asm dec cx;
/* Add the next 64 bytes of the packet into the checksum */
       __asm adc dx, es:word ptr [di + 62];
       __asm adc dx, es:word ptr [di + 60];
       __asm adc dx, es:word ptr [di + 58];
       __asm adc dx, es:word ptr [di + 56];
       __asm adc dx, es:word ptr [di + 54];
       __asm adc dx, es:word ptr [di + 52];
       __asm adc dx, es:word ptr [di + 50];
       __asm adc dx, es:word ptr [di + 48];
       __asm adc dx, es:word ptr [di + 46];
       __asm adc dx, es:word ptr [di + 44];
       __asm adc dx, es:word ptr [di + 42];
       __asm adc dx, es:word ptr [di + 40];
       __asm adc dx, es:word ptr [di + 38];
       __asm adc dx, es:word ptr [di + 36];
       __asm adc dx, es:word ptr [di + 34];
       __asm adc dx, es:word ptr [di + 32];
       __asm adc dx, es:word ptr [di + 30];
       __asm adc dx, es:word ptr [di + 28];
       __asm adc dx, es:word ptr [di + 26];
       __asm adc dx, es:word ptr [di + 24];
       __asm adc dx, es:word ptr [di + 22];
       __asm adc dx, es:word ptr [di + 20];
       __asm adc dx, es:word ptr [di + 18];
       __asm adc dx, es:word ptr [di + 16];
       __asm adc dx, es:word ptr [di + 14];
       __asm adc dx, es:word ptr [di + 12];
       __asm adc dx, es:word ptr [di + 10];
       __asm adc dx, es:word ptr [di + 8];
       __asm adc dx, es:word ptr [di + 6];
       __asm adc dx, es:word ptr [di + 4];
       __asm adc dx, es:word ptr [di + 2];
       __asm adc dx, es:word ptr [di];
/*
 * adc (add with carry) works by setting the carry bit if there's a carry, and
 * then picking it up on the next adc instruction. We execute one final adc
 * here to pick up the carry bit
 */
       __asm adc dx, 0;
/* Add 64 to the offset */
       __asm add di, 64;
/* Go back to the top of the loop */
       __asm jmp TL_CHECKSUM_LOOP_TOP;
TL_CHECKSUM_LOOP_END:
/* Copy the sum out of dx and back into sum16 */
       __asm mov sum16, dx;
/* Restore all the registers that we used */
       __asm pop cx;
       __asm pop di;
       __asm pop dx;
       __asm pop es;
/* Increment the pointer to the correct point */
       link16BitDataPtr += (linkLength >> 1) - switchOffset;
/*
 * We're done with the 16-bit variable. Move the sum back to the standard
 * (32-bit) variable for the rest of the function
 */
       sum = (tt32Bit)sum16;
/* We need to know if linkLength was odd */
       linkLength &= 1;
       if (sumByteSwapped != TM_8BIT_ZERO)
       {
/*
 * We want to add the saved even byte, so byte swap the sum to start
 * collecting the even bytes.
 */
           tm_byte_swap_sum(sum);
/* toggle byte swapping */
           sumByteSwapped = TM_8BIT_ZERO;
           if (linkLength != 0)
/* extra byte at the end. We can pair it with our saved even byte */
           {
               oddByte16Bit.oddChar[1] = *((tt8BitPtr)link16BitDataPtr);
/* add to sum */
               sum = sum + oddByte16Bit.oddWord;
               linkLength = 0;
           }
           else
           {
/* remember that we have our even byte stored in oddChar[0] */
               linkLength = 1;
           }
       }
       else
       {
           if (linkLength != 0)
           {
/* Odd byte length. Save the character to add it later on */
               oddByte16Bit.oddChar[0] = *((tt8BitPtr)link16BitDataPtr);
           }
       }
/* check this before computing next packetPtr */
       if (totalDataLength == (ttPktLen)0)
       {
/* break out of the loop. Do not check 0 length after the loop */
           goto outFold;
       }
       packetPtr = (ttPacketPtr)packetPtr->pktLinkNextPtr;
   } while (packetPtr != TM_PACKET_NULL_PTR);
#ifdef TM_ERROR_CHECKING
/* double check that all data has been checksumed */
   if (totalDataLength != (ttPktLen)0)
   {
       tfKernelError("tfPacketChecksum",
               "Data in Packet chain smaller than length to be checksumed");
   }
#endif
outFold:
   if (linkLength != 0UL)
   {
/*  Add left-over byte */
       oddByte16Bit.oddChar[1] = 0;
       sum = sum + oddByte16Bit.oddWord;
   }
/*  Fold 32-bit sum to 16 bits, adding posssible carries from fold */
   tm_add_carries_sum(sum);
   return (tt16Bit)~sum;
}
THANK YOU!
0 Kudos
Reply

2,875 Views
mccPaul
Contributor I
Hi
 
The CF instructions that are used as equivalents of push and pop are link and unlink.
 
Link is used to store the current stack pointer in a register and to then create space on the stack. When the space is created, you can copy register contents to the stack:
 
Code:
   link %a6, #-16   movem.l %d2-%d3/%a1-%a2, (%sp) // push d2, d3, a1 & a2   ... Do something   movem.l (%sp),%d2-%d3/%a1-%a2 // restore d2, etc now we are done with them   unlk %a6

 

The example above puts the current sp into a6 and reserves 16 bytes on the stack. the movem instruction copies the d2, d3, a1 and 2 registers to the reserved space. You could obviously copy different registers here. If you need more or less space (each register is 4 bytes) then you adjust the link instruction.

The shift, add, & and instructions in your first post have direct equivalents in CF assembler.The les instruction does not. See the CF reference manual: http://www.freescale.com/files/dsp/doc/ref_manual/CFPRM.pdf for all CF instructions.
 
There are several assembly code samples on the MCF5307 product page. If you want to find an example of checksum code look at the DBUG source or NicheLite sample for the MCF5223x.
 
Cheers,
 
Paul.
 
0 Kudos
Reply

2,875 Views
Veter
Contributor I
Thank you very much for your answer. My code replacement looks like:
 asm
  {
   link a7, #-16
   movem.l es/di/dx/cx,(a7)
  }
 
The movem.l does not compile, the error said "illegal addressing" and points to the '/' character.
How can I push this registeres into a7?
0 Kudos
Reply

2,875 Views
mccPaul
Contributor I
Hi Veter,
 
You have more than one problem. The "illegal addressing" error happens because the es register does not exist in the Coldfire so the assembler does not understand it, plus you have misunderstood the movem instruction.
 
The code you are trying to port is for an entirely different CPU. This not only means that the instructions are different, but the available registers are also different. es/di/dx/cx are not Coldfire registers. The Coldfire has eight data registers, d0 to d7 and eight address registers a0 to a7. You need to rewrite your code to use Coldfire registers.
 
The link instruction copies the current stack pointer into the register you specify and then subtracts the number of bytes that you specify from the stack pointer. The movem instruction is used to copy the specified registers to the current stack pointer address. This is the same as using the Intel push instruction to push registers onto the stack. The end result is that the register contents are stored on the stack and the stack pointer is adjusted by the number of bytes that are stored.
 
Your code should be more like:
 
Code:
asm  {   link %a7, #-16   movem.l %d0-%d3,(%sp)  }

 
Assuming you are using registers d0 to d3. The % can be omitted for some assemblers.
 
Paul.
0 Kudos
Reply

2,875 Views
Veter
Contributor I
Thank you, Paul, very much!
It works.
0 Kudos
Reply