apparent Lite web server memory leak with M52233 demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

apparent Lite web server memory leak with M52233 demo board

2,039 Views
spooky
Contributor I
Have been running the demo in the ajax_bargraph_demo directory. It seems to work OK intially, but I've been leaving it running for times not quite upto an hour and finding that the updates to the browser have ceased.
 
I've also been using the console memory command that seems to output the heap parameters among other things. The values for min and current start above 4000 and seem to gradually decline over time until the web server fails. The amounts listed when it has failed vary each time, sometimes still over 1000, sometimes actually what appear to be negative 32-bit values.
 
This is the code that was distributed at a seminar for this demo board back in 5/06. I'm wondering if there's an update or patch for this...
Labels (1)
0 Kudos
Reply
1 Reply

1,184 Views
DrSeuss
Contributor I
The lastest releases are at www.freescale.com/coldfireseminars
I'm not sure what the current version currently posted is but I know there will be a new posting this week or early next week. There have been lots of enhancements and changes. Though I have not heard of this.
0 Kudos
Reply