a 6x4 matrix in framebuffer is modified by others

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

a 6x4 matrix in framebuffer is modified by others

1,708 Views
yanchzh
Contributor I

   I am using the ltib-nommu-20081218 version of BSP for MCF5329,with a 480x272 LCD panel .But there is a black rectangle at the coordinate (0,84), 4 pixel width and 6 pixel heigh.I just used two method to write the framebuffer.One method is open /dev/fbo,lseek,then write 0xffffffff ,after all buffer is wrote,then read the buffer and print readed data,in the rectangle the is 0.After write 0xffffffff,the code read the same address,the data is still 0xffffffff.But when all buffers is wrote,the data in the rectangle is modified.Another method is using mmap,it is the same.

  I tried to modified the linux/drivers/video/mcf-fb.c file cutting off all hardware related code.It is the same conclusion.

  Anyone who met the problem tell me how to resolve it.

Labels (1)
0 Kudos
Reply
1 Reply

1,292 Views
J2MEJediMaster
Specialist I

I checked with one of our Linux/BSP people here and he suggests that you file a service request on this problem. Click here to be directed to the sevice request page.

 

---Tom

0 Kudos
Reply