Why External Phy?!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why External Phy?!

6,778件の閲覧回数
rdazcal
Contributor III

Please excuse my ignorance:

 

Why is it that most freescale's MCUs use external PHY instead of internal PHY like the MCF5223x family?

 

Is it to offer the possibility to connect to means of communications other than Ethernet?

 

I thank you in advance.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,207件の閲覧回数
gmnelson
Contributor III

Good question!  I have a couple reasons "why an external PHY?"

 

An external PHY gives our company the opportunity to provide a Fiber ethernet connection as well as the standard copper ethernet option.

 

Also, an external PHY gives us the ability to 'ruggedize' the ethernet input hardware.  That is we can add circuitry (transorbs etc.) that protects against harsh environments where voltage spikes and transients happen regularly.

0 件の賞賛
返信

4,207件の閲覧回数
rdazcal
Contributor III

Thank you gmnelson

0 件の賞賛
返信

4,207件の閲覧回数
scifi
Senior Contributor I

I was thinking the same thing.

If MCF5225x had a built-in Ethernet PHY, it would be almost perfect for my current application.

But I have to say that the PHY in MCF5223x has its drawbacks. It's too power-hungry, auto-negotiation is broken, missing automatic MDI/MDI-X detection.

There must be some cost associated with a built-in Ethernet PHY. Substantial silicon area, could interfere with the ADC, maintaining or licencing a PHY has a cost too. I'm just speculating here, though...

0 件の賞賛
返信