Where is the library for the "Digital Signal Processing Libraries Using the ColdFire ® eMAC and MAC"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the library for the "Digital Signal Processing Libraries Using the ColdFire ® eMAC and MAC"?

ソリューションへジャンプ
1,817件の閲覧回数
yibbidy
Contributor V

This library is thoroughly documented in this document http://www.freescale.com/files/32bit/doc/ref_manual/DSPLIBUM.pdf:

 

Digital Signal Processing Libraries

Using the ColdFire® eMAC and MAC

User’s Manual

DSPLIBUM

Rev. 1.2

03/2006

 

... but I cannot find the accompanying library file anywhere.  The closest that I can get is this page: CFDSPLIB: Complimentary ColdFire Digital Signal Processing Library which also has no download.  It appears that you set up your high/low/band pass filter parameters here, and then download an XML file which mentions signal processing .c and .h files, but the files are not provided.  Also, this page only has band pass/stop filters, whereas the library I am looking for has FFT, FIR and IIR.

 

Does anyone have a link to download these files?

 

Thanks,

 

Shaun

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,452件の閲覧回数
yibbidy
Contributor V

It turns out that the DSP library is available here http://cache.freescale.com/files/32bit/doc/ref_manual/DSPLIBUMSW.zip, but needs work to compile on CW 7.2 and above.

I'd still like to find the code for the filters in the library referred to at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CFDSPLIB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,453件の閲覧回数
yibbidy
Contributor V

It turns out that the DSP library is available here http://cache.freescale.com/files/32bit/doc/ref_manual/DSPLIBUMSW.zip, but needs work to compile on CW 7.2 and above.

I'd still like to find the code for the filters in the library referred to at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CFDSPLIB

0 件の賞賛
返信