Wake up from Stop3 Mode by SCI interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wake up from Stop3 Mode by SCI interrupt

1,684 次查看
sssampath
Contributor I

hi,

      In my code i kept the controller into stop3 mode. its not coming out of stop mode through SCI interrupt.its working with RTC.but we need the wake up by SCI interrupt.is wakeup is possible through SCI interrupt.

标签 (1)
0 项奖励
回复
3 回复数

1,065 次查看
TomE
Specialist II

Which CPU? Coldfire 1, 2, 3 or 4?

 

Assuming you're using something like an MCF51CN128, do you have RXEDGIE set properly?

 

 

13.3.5.2      Stop Mode OperationDuring all stop modes, clocks to the SCI module are halted....The receive input active edge detect circuit remains activein stop3 mode, but not in stop2. An active edge on thereceive input brings the CPU out of stop3 mode if theinterrupt is not masked (RXEDGIE = 1).

 

 

0 项奖励
回复

1,065 次查看
Jigs_esenza
Contributor I

Setting RXEDGIE Can make it work, wake up is possible. I faced one more issue after setting it, the TX interrupts are not being generated. All settings are really correct (checked using BDM), still dont know why TX interrupt doesnot come?

 

Any Idea on this ?

0 项奖励
回复

1,065 次查看
TomE
Specialist II

No, sorry. Have you tried reprogramming the SCI from scratch?

0 项奖励
回复