VSTBY pin, when not used

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VSTBY pin, when not used

3,309件の閲覧回数
efk
Contributor I
Hello,

I have a question regarding VSTBY pin of M5221x.
When we do not wish to use the standby power feature (i mean no battery on printed circuit board), i do not understand where to connect this pin.

Shall i connect it to 3,3V ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,261件の閲覧回数
efk
Contributor I
After a Google research, i found this text in another PDF file (Freescale MPC5565 Microcontroller Data Sheet): "If standby operation is not required, VSTBY can be connected to ground"

So i think there is a good chance it is the same with the M5221x (?)



Message Edited by efk on 2008-09-26 09:07 AM
0 件の賞賛
返信

2,261件の閲覧回数
efk
Contributor I
Could you please tell my if my above question is dummy, or do the M5221x users always include the battery for VSTBY in their production pcb ?

0 件の賞賛
返信

2,261件の閲覧回数
efk
Contributor I
After more research, i found another Freescaler processor PDF file which says: "If standby operation is not required, connect VSTBY  to ground". It is the MPC5554 data sheet.
I will do the same with the M5221x.

0 件の賞賛
返信