V1 USB CDC Rx 64 byte msg (without locking up)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

V1 USB CDC Rx 64 byte msg (without locking up)?

1,431 Views
Kerrie
Contributor I

We are using the JE256 ColdFire V1 part and codewarrior 6.3 to make used of the USB phcp demo for CDC.

We can successfully recieve 1 message over USB that is 64 bytes in length and then send and ACK which is 1 byte in length, after that the micro code continues to run, but no matter what I send from the PC to the mico I can't get theVirtual_Com_App function to see that a new message has been transmitted.

 

Thanks, Kerrie

Labels (1)
0 Kudos
Reply
1 Reply

1,244 Views
Kerrie
Contributor I

Bump,  anyone have any ideas.....

0 Kudos
Reply