Upload file from web server to a 52235EVB board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upload file from web server to a 52235EVB board

1,474件の閲覧回数
fjoli
Contributor I
Hello,

I work on the board 52235EVB with codewarrior V7.0 and I am using the ColdFire TCP/IP Lite by InterNiche.

I would like to know if it is posible to upload a file from the web server to the board in order to load this file in an extern flash memory.
So I want to upload a file packet by packet in order to have the time to tranfert each packet to the extern memory flash.

I would like to do this in order to load a new application to the extern flash memory to load to the intern flash memory on the following reset.

Does anyone have an idea to do that ?

Thanks

Fabien
ラベル(1)
0 件の賞賛
返信
1 返信

734件の閲覧回数
NT
Contributor I
Hi Fabian
 
I haven't worked with external flash memory but I was able to store the contents from webpage to the flash memory. 
 
NT
0 件の賞賛
返信